reComputer J4012 (OrinNX 16GB) - JetPack 6.1 and 6.2

Hi all.
I’ve tried JP 6.2 and 6.1 and still the same:
I Can’t upgrade it.

I always get an error when apt is trying to update nvidia-l4t-* packages:

ERROR. 3767-000-0000--1--recomputer-orin-j401- does not match any known boards.
dpkg: error processing package nvidia-l4t-bootloader (--configure):
 installed nvidia-l4t-bootloader package post-installation script subprocess returned error exit status 1
Setting up nvidia-l4t-kernel (5.15.148-tegra-36.4.7-20250918154033) ...
Using the existing boot entry 'primary'
Warning: Cannot get compatible board name.
3767-000-0000--1--recomputer-orin-j401-
TNSPEC 3767-300-0000-M.1-1-0-recomputer-orin-j401-
COMPATIBLE_SPEC 3767-000-0000--1--recomputer-orin-j401-
TEGRA_BOOT_STORAGE nvme0n1
TEGRA_CHIPID 0x23
TEGRA_OTA_BOOT_DEVICE /dev/mtdblock0
TEGRA_OTA_GPT_DEVICE /dev/mtdblock0
Info: Write TegraPlatformCompatSpec with 3767-000-0000--1--recomputer-orin-j401-.
Info: The esp is already mounted to /boot/efi.
Starting kernel post-install procedure.
Rootfs AB is not enabled.
ERROR. Procedure for A_kernel update FAILED.
Cannot install package. Exiting...
dpkg: error processing package nvidia-l4t-kernel (--configure):
 installed nvidia-l4t-kernel package post-installation script subprocess returned error exit status 1
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-headers:
 nvidia-l4t-kernel-headers depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.7-20250918154033); however:
  Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-kernel-headers (--configure):
 dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-jetson-io:
 nvidia-l4t-jetson-io depends on nvidia-l4t-kernel (>> 5.15.148-tegra-36.4-0); however:
  Package nvidia-l4t-kernel is not configured yet.
 nvidia-l4t-jetson-io depends on nvidia-l4t-kernel (<< 5.15.148-tegra-36.5-0); however:
  Package nvidia-l4t-kernel is not configured yet.

No apport report written because the error message indicates its a followup error from a previous failure.
                                                                                                          No apport report written because MaxReports is reache
d already
         dpkg: error processing package nvidia-l4t-jetson-io (--configure):
 dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-oot-modules:
 nvidia-l4t-kernel-oot-modules depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.7-20250918154033); however:
  Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-kernel-oot-modules (--configure):
 dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-display-kernel:
 nvidia-l4t-display-kernel depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.7-20250918154033); however:
  Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-display-kernel (--configure):
 dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-oot-headers:
 nvidia-l4t-kernel-oot-headers depends on nvidia-lNo apport report written because MaxReports is reached already
                                                                                                                No apport report written because MaxReports is 
reached already
               No apport report written because MaxReports is reached already
                                                                             4t-kernel (= 5.15.148-tegra-36.4.7-20250918154033); however:
  Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-kernel-oot-headers (--configure):
 dependency problems - leaving unconfigured
dpkg: dependency problems prevent configuration of nvidia-l4t-kernel-dtbs:
 nvidia-l4t-kernel-dtbs depends on nvidia-l4t-kernel (= 5.15.148-tegra-36.4.7-20250918154033); however:
  Package nvidia-l4t-kernel is not configured yet.

dpkg: error processing package nvidia-l4t-kernel-dtbs (--configure):
 dependency problems - leaving unconfigured
No apport report written because MaxReports is reached already
                                                              Processing triggers for nvidia-l4t-initrd (36.4.7-20250918154033) ...
Include /etc/nv-update-initrd/list.d/binlist
Include /etc/nv-update-initrd/list.d/modules
nv-update-initrd: Updating /boot/initrd from /etc/nv-update-initrd/list.d for kernel version 5.15.148-tegra..
Add /usr/sbin/nvluks-srv-app
Add /lib/modules/5.15.148-tegra/updates/drivers/net/ethernet/nvidia/nvethernet/nvethernet.ko
Add /lib/modules/5.15.148-tegra/updates/drivers/nvpps/nvpps.ko
Add /lib/modules/5.15.148-tegra/updates/drivers/net/ethernet/realtek/r8126/r8126.ko
Add /lib/modules/5.15.148-tegra/updates/drivers/net/ethernet/realtek/r8168/r8168.ko
Add /lib/modules/5.15.148-tegra/modules*
Add /lib/modules/5.15.148-tegra/kernel/drivers/nvme/host/nvme.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/nvme/host/nvme-core.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/thermal/tegra/tegra-bpmp-thermal.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/pwm/pwm-tegra.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/hwmon/pwm-fan.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/pci/controller/dwc/pcie-tegra194.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/phy/tegra/phy-tegra194-p2u.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/gadget/udc/tegra-xudc.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/typec/ucsi/typec_ucsi.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/typec/ucsi/ucsi_ccg.ko
Add /lib/modules/5.15.148-tegra/kernel/drivers/usb/typec/typec.ko
Updating modprobe.d configuration directories for modprobe..
Add config /etc/modprobe.d/alsa-base.conf
Add config /etc/modprobe.d/bcmdhd.conf
Add config /etc/modprobe.d/blacklist-ath_pci.conf
Add config /etc/modprobe.d/blacklist.conf
Add config /etc/modprobe.d/blacklist-firewire.conf
Add config /etc/modprobe.d/blacklist-framebuffer.conf
Add config /etc/modprobe.d/blacklist-modem.conf
Add config-link /etc/modprobe.d/blacklist-oss.conf
Add config /etc/modprobe.d/blacklist-rare-network.conf
Add config /etc/modprobe.d/denylist-nouveau.conf
Add config /etc/modprobe.d/denylist-oot-modules-audio.conf
Add config /etc/modprobe.d/denylist-ramoops.conf
Add config /etc/modprobe.d/denylist-tegra-safety.conf
Add config /etc/modprobe.d/denylist-tpm-ftpm-tee.conf
Add config /etc/modprobe.d/iwlwifi.conf
Add config /etc/modprobe.d/nvgpu.conf
Add config /etc/modprobe.d/nvidia-display.conf
Add config /etc/modprobe.d/tegra-udrm.conf
Add config /lib/modprobe.d/aliases.conf
Add config /lib/modprobe.d/fbdev-blacklist.conf
Add config /lib/modprobe.d/systemd.conf
Cleaning up the temporary directory for updating the initrd..
Errors were encountered while processing:
 nvidia-l4t-bootloader
 nvidia-l4t-kernel
 nvidia-l4t-kernel-headers
 nvidia-l4t-jetson-io
 nvidia-l4t-kernel-oot-modules
 nvidia-l4t-display-kernel
 nvidia-l4t-kernel-oot-headers
 nvidia-l4t-kernel-dtbs
E: Sub-process /usr/bin/dpkg returned an error code (1)

Is there any solution to this ?
This is affecting the use of Nvidia

Thank you

Hi there,

So I see it’s been a whil since you were last here, A lot has changed, but the Clones are just that Clones , but not Exact clones. If you keep looking and reading you will arrive at the conclusion. You can’t use Nvidia stuff to update or Upgrade these units. The Device tree files and other portions, like WiFi and HDMI are Not the same.

Read up on how exactly to go about it and in the other threads are some links AFAIK to the “Other” stuff needed to make the jump from JetPack to JetPack a thing. :+1:

HTH
GL :slight_smile: PJ :v:

Hi !
I’m not around the forum, but I’m on discord. :slight_smile:
I know this are SeeedStudio’s “ports” and some stuff is not the same.

The thing is, this is affecting, not only JP 6.2 but also 6.1 .
I’ve installed JP 6.0 and it seems to be working.
If this is not ready for production and Seeed knows this, why do they make available those versions ?
They know people are going to install and try them . :slight_smile:

I think they should only make them available when they are ready for production.
But hey, thank you Seeed to make this available.

Hi there,

Well , let’s just say the Documentation sometimes LAgs :grin: the users base requests…to make stuff work. I agree with you but it’s changing so fast if you sleep on it the next week it;'s something different :stuck_out_tongue_winking_eye:

I think 6.1 started the Supermode compatibility tree requirement or something I’ve been told. That is why 6 was a plug and play pretty much , though some did have issue’s with Wifi if they had updated to a later driver, and the latest HDMI wasn’t included and the carry over was Nurf’d up so Folks saw issues there.
Stay with it and stay calm , they will come through. I like they are just coming of a holiday so be patient. :crossed_fingers:

HTH
GL :slight_smile: PJ :v:

It is great hardware though for the price, just the clone part is biting a little. YMMV