A new problem with “Compatibility Issue between reComputer and VEYE Camera”, with the new reComputer J4011B
The old topic (VEYE IMX462 I2C address detection on the J401 carrier board) was solved by the J401 carrier board USB hub firmware fix (updating FW Version 07F3 to Version 08B3):
Solution for the Compatibility Issue between reComputer and VEYE Camera | Seeed Studio Wiki
However, it seems to have come back with the new reComputer J4011B (at least with Jetpack V6.2, I have not tested other versions of Jetpack so far).
The Veye camera driver loads (IMX462), but the camera I2C address is not detected.
And this is even though the J4011B carrier board has the USB hub firmware fix preinstalled (FW Version 08B3). Perhaps this is a result of the USB change, i.e., two of the J401 USB external ports have been replaced by one internal USB port for a mini-PCIe adapter “extension board”.
Could there be a solution for the Veye camera on the reComputer J4011B?
Thanks
John