I am struggling to find a clear answer to what is the maximum input voltage of these new J202 carrier boards. There are some mentions of it being 16V in the docs, while an image of the board here shows 9V-12V on the silkscreen: reComputer J2021-Edge AI Device with Jetson Xavier NX 8GB module, 4xUSB, M.2 Key E & Key M Slot, Aluminum case, Pre-installed JetPack System - Seeed Studio
My device uses a 19V input, and I need to know if this is compatible with the product in that link above.
I’ve got several J2012 devices here already but they’re not in stock at the moment for me to buy more. Is Seeed phasing out this older J201 carrier board?