Hello, I have ran into a problem with my reComputer J1010 where it gets stuck on bootup with the final message being:
[OK] Started User Manager for UID 120.
Before this error, I had successfully performed a memory expansion on my J1010 a few weeks before encountering this bootup error. During these few weeks, I could use my device with no problems.
However, the other day before shutting down my device, I received a red “stop light” icon in the top right of the task bar indicating that I had “installed packages with unmet dependencies”. However, I did not resolve these dependency issues before shutting off my reComputer. Although, I do know they were related to the NVIDIA driver 465.
Now, when I go to bootup my reComputer, it hangs on the error message above. Below, I will attach screenshots of some of the other bootup logs. I do not know how to bring up the terminal during bootup to resolve the dependency issues (is this even possible?). Likewise, I have no other functionality. I have searched elsewhere, and it seems my only option is to perform a force recovery mode in order to reinstall the JetPack OS.
Also, since I cannot bootup the device, I cannot ssh into the device from my host machine. Any help would be greatly appreciated.