Hi,
SD card slot is not working on my reComputer J1020 with Jetson Nano module. I have tried inserting 64gb SD card through SD Card Reader and it’s getting detected so there’s no issue with the SD Card.
Thank you.
Hi,
SD card slot is not working on my reComputer J1020 with Jetson Nano module. I have tried inserting 64gb SD card through SD Card Reader and it’s getting detected so there’s no issue with the SD Card.
Thank you.
First, find your SD card in “Device Manager” and right-click it. If it shows “Disable Device”, then you have already enabled the SD card reader and there is no need to do anything. If not, just select the option “Enable Device”. Then Windows 10 could detect your SD card usually.
Regards,
Peter
Hi Peter,
Thanks for your response.
Actually, I am not using the Jetson Nano on headless mode. So, there is no problem in the SD card.