Hi,
I followed the quick start guide for reCamera I was able to get it up and running in no time using the pre-built Node-RED dashboard with the example provided on the youtube video.
However, if I make the node-red flow a little bit more complex, e.g., by adding a http request block, the node-red module stops working completely and a factory reset is needed.
Do you have any additional example I can follow?
Thanks
Hi - were you able to make Node-RED work beyond the simple example that reCamera comes with?
I have the same issue, it will reboot or just freeze if you add some simple flows. Even the simple example that comes with it causes the video and processing to freeze every 30 secs or so. The YT below is not helpful, I watched all 40mins and he only describes his top ten best applications with Node-RED and doesn’t address freezing or rebooting when you try to run simple flows in Node-RED.
Thanks
The last sw update solved the issue for me
Thanks @warner83 for following up - did you mean the reCamera OS sw update or the Node-Red sw update?
Thanks
Anno
Actually, I updated it all and its definitely better - thanks for the advise earlier.