I tried to install Ubuntu 20.04 on my ODYSSEY-X86J4105 (with Windows 10 pre-loaded). But, half way through (write after setting the time zoon), my installation crashed. It seems that the processor could not write the image on the ssd. I installed additional SSD (970 EVOPLUS), and I tried it again. Still processor could not write the image on this SSD also. Now, I cannot boot Windows also. Is there any way I access windows 10 again?