To tech support
From: info info@florian-denz.de
Date: Monday, March 18, 2019 at 1:38 AM
To: iot@seeed.cc
Subject: CAN-Bus Shield V1.2 Libary
Resent-From: iot@seeed.cc
Resent-To: shuyang@seeed.cc
Resent-Date: Mon, 18 Mar 2019 01:38:20 +0800 (CST)
Hello,
I bought a CAN-Bus Shield over a distributor a few years ago. I wrote a own libary to communicate with over devices over the CAN bus.
Now I would like to use your libary to test especially the OBD-II example code.
In the readme file on the github page only the CAN-Bus Shield V2.0 is named. Is this libary also compatible with the old version of the Shield (V1.2)?
I really looking forward to hearing from you.
Mit freundlichen Grüßen/Best regards,
Florian Denz
Electrical Engineering Student in Germany