[Question] Grove Indoor Environment kit wrong sensor values

Hi ,

I just bought grove indoor environment kit for intel edison

followed the instructions mentioned in manual to connect the sensors .
I see wrong values reported . Attached screen shot from the demo sketch

Could you see what is is that I am doing wrong
All the grove modules are plug and and play right ?
I am using intel edison booted from an sdcard .

Hi,

The following code will resolve your issue.

#include <Servo.h>
#include <SPI.h>
#include <WiFi.h>
#include <TimerOne.h>
#include "rgb_lcd.h"
#include <stdlib.h>
#include <string.h>
#include <TH02_dev.h>


#define CMDSTR_MAX_LEN (128)
#define LOW_TEMP       (10)
#define NOM_TEMP       (25) 
#define HIGH_TEMP      (40)

#define SENSOR_COUNT   (6)
#define ACTUATOR_COUNT (4)
#define VAR1_COUNT     (SENSOR_COUNT+1)
#define VAR2_COUNT     (ACTUATOR_COUNT+1)
typedef void (*pActuatorHandler)(int);
typedef int (*pgetSensorValue)(void);

rgb_lcd lcd;
boolean isBackLightOn = true;

char cmdstr[CMDSTR_MAX_LEN];

char ssid[48] = "EdisonAP";           // your network SSID (name) 
char psw[48] = "12345678";       // your network password
boolean isSSIDreconfiged = false;
int keyIndex = 0;                // your network key Index number (needed only for WEP)
int status = WL_IDLE_STATUS;
WiFiServer server(88);
int serverconnected = 0;

unsigned char BLColorRGB[]={0x00, 0x00, 0xFF};  //Backlight color

const int numRows = 2;
const int numCols = 16;

const int MenuCount = 5;
int MenuIndex = 0;

const int MoistrueSensorIndex = 0;
const int LightSensorIndex = 1;
const int UVSensorIndex = 2;
const int THSensorIndex = 3;
const int LocalIPIndex = 4;

const int pinSound = A0;
const int pinMoistrue = A1;
const int pinLight = A2;
const int pinUV = A3;
const int pinButton =0;
const int pinEncoder1 = 2;
const int pinEncoder2 = 3;
const int pinBuzzer = 4;
const int pinRelay = 5;
const int pinPIR = 7;
const int pinServo = 6;
Servo myservo;

const char* SerialVarList1[] = { "temp", "humi", "light", "uv", "pir", "ms","ssid"};
const char* SerialVarList2[] = { "relay", "buzzer", "servo", "sleep", "psw"};
enum ACTUATOR {RELAY=0,BUZZER,SERVO,SLEEP};
enum SENSOR {TEMPER=0,HUMI,LIGHT,UV,PIR,MS};

pgetSensorValue getSensorValueList[]={
  getTempSensorValue, 
  getHumiSensorValue, 
  getLightSensorValue, 
  getUVSensorValue, 
  getPIRSensorValue, 
  getMoistrueSensorValue
};

int SensorValue[SENSOR_COUNT];
                                      
pActuatorHandler ActuatorHandlerList[]={RelayHandle, BuzzerHandle, ServoHandle, SleepHandle};

int SensorConfig[][4] = {       // value, condition, Actuator, action
  {85,  '>', SLEEP,  1},        //Temperature
  {100, '>', SLEEP,  1},        //Humdity
  {200, '<', SERVO,  90},        //Light
  {1023,'>', SLEEP,  1},        //UV
  {2,   '=', BUZZER, 1},        //PIR
  {600, '<', RELAY,  1}         //Moistrue
};

void printSettings(void){
  Serial.println("The Sensors Configurations as follow:");
  for(int i=0; i<SENSOR_COUNT;i++){
    Serial.print(SerialVarList1[i]);
    Serial.write((char)SensorConfig[i][1]);
    Serial.print(SensorConfig[i][0]);
    Serial.write(',');
    Serial.print(SerialVarList2[SensorConfig[i][2]]);
    Serial.write('=');
    Serial.println(SensorConfig[i][3]);    
  }
  Serial.print('\n');
  Serial.print("SSID = ");
  Serial.print(ssid);
  Serial.print(", PSW = ");
  Serial.println(psw);
  
  Serial.println("The Sensors Value as follow:");
  for(int i=0; i<SENSOR_COUNT;i++){
    Serial.print(SerialVarList1[i]);
    Serial.print(" = ");
    Serial.println(getSensorValueList[i]());   
  }
}

void SerialRequestHandler(){
  if(cmdstrInput(cmdstr)){
     Serial.println(cmdstr);
     if(!parsecmd(cmdstr)){
       Serial.println("  ---- FAIL!");
       Serial.println("Please enter command: set temp>50,relay=1 etc.");
     }
     else {
       Serial.println("  ---- OK!");
     }
     printSettings();
  }
  int changedVal;
  for(int i=0;i<SENSOR_COUNT;i++){
    if(SensorConfig[i][2]==SERVO) changedVal = 0;
    else changedVal = !SensorConfig[i][0];
    switch (SensorConfig[i][1]){
      case '>':
        if(getSensorValueList[i]() > SensorConfig[i][0]) 
          ActuatorHandlerList[SensorConfig[i][2]](SensorConfig[i][3]);
        else ActuatorHandlerList[SensorConfig[i][2]](changedVal);
        break;
      case '<':
        if(getSensorValueList[i]() < SensorConfig[i][0]) 
          ActuatorHandlerList[SensorConfig[i][2]](SensorConfig[i][3]);
        else ActuatorHandlerList[SensorConfig[i][2]](changedVal);
        break;
      case '=':
        if(getSensorValueList[i]() == SensorConfig[i][0]) 
          ActuatorHandlerList[SensorConfig[i][2]](SensorConfig[i][3]);
        else ActuatorHandlerList[SensorConfig[i][2]](changedVal);
        break;
    }
  }
}

int parsecmd(char *cmd){
  char* cp = cmd;

/*  // use SSID and Passwrod, should not changed to lowcase
  while(*cp != '\0'){
    if(*cp >= 'A' && *cp <= 'Z') *cp += 0x20;     //tolower
    cp++;
  }
*/
  
  if(!(cmd[0]=='s' && cmd[1]=='e' && cmd[2]=='t' && cmd[3]==' ')) return 0;   //Illegal cmd
  
  char tmpcmd[CMDSTR_MAX_LEN];
  char *cp1=cmd+4;
  int len=0;
  while(*cp1 != '\0'){
    if(*cp1 != ' ') tmpcmd[len++] = *cp1;   //delete space
    cp1++;
  }
  tmpcmd[len]='\0';
  if(len<7) return 0;   // at least 7 characters,like T>0,R=1
  
  char *pvar1, *pvar2;
  pvar1 = strtok(tmpcmd,",");
  if(pvar1 == NULL) return 0;          //no setting
  pvar2 = strtok(NULL,",");
  if(pvar2 == NULL) return 0;          //no setting
  if(strtok(NULL,",")!=NULL) return 0; //more setting
  
  char op1='\0',op2='\0';
  char *pvarvalue1=NULL, *pvarvalue2=NULL;
  int i = 0;
  while(pvar1[i]!='\0'){
    if(pvar1[i]=='>' || pvar1[i]=='<' || pvar1[i]=='='){
      op1 = pvar1[i];
      pvar1[i] = '\0';
      pvarvalue1 = pvar1+i+1;
      break;
    }
    i++;
  }
  i=0;
  while(pvar2[i]!='\0'){
    if(pvar2[i]=='>' || pvar2[i]=='<' || pvar2[i]=='='){
      op2 = pvar2[i];
      pvar2[i] = '\0';
      pvarvalue2 = pvar2+i+1;
      break;
    }
    i++;
  }
  int varindex1,varindex2;
  for(i=0;i<VAR1_COUNT;i++)
    if(strcmp(pvar1,SerialVarList1[i])==0){
      varindex1 = i;
      break;
    }
    
  if(i==VAR1_COUNT) return 0;  // Illegal sensor name
  
  for(i=0;i<VAR2_COUNT;i++)
    if(strcmp(pvar2,SerialVarList2[i])==0){
      varindex2 = i;
      break;
    }
    
  if(i==VAR2_COUNT) return 0; // Illegal actuator name
  
  if(op1=='\0' || op2=='\0') return 0; // Illegal operator name
  
  if(varindex1 == VAR1_COUNT-1 && varindex2 == VAR2_COUNT-1){
    strcpy(ssid,pvarvalue1);
    strcpy(psw,pvarvalue2);
    isSSIDreconfiged = true;
  } 
  else if(varindex1 != VAR1_COUNT-1 && varindex2 != VAR2_COUNT-1) {
    int value1 = atoi(pvarvalue1), value2 = atoi(pvarvalue2);
    if(value1 < 0 || value1 > 1023) return 0;
    if(value2 < 0 || value2 > 1023) return 0;  
    SensorConfig[varindex1][0] = value1;
    SensorConfig[varindex1][1] = op1;
    SensorConfig[varindex1][2] = varindex2;
    SensorConfig[varindex1][3] = value2;
  }
    
  return 1;
}


//get Grove-Sound Sensor value
int getSoundSensorValue(){
    return analogRead(pinSound);
}
//get Temperature Senso value
int getTempSensorValue(){
  delay(150);
  /* Reset HP20x_dev */
  TH02.begin();
  delay(100);
  int temper =(int) TH02.ReadTemperature();
  SensorValue[TEMPER] = temper;
  return temper;
}

//get Humidity Senso value
int getHumiSensorValue(){
   delay(150);
  /* Reset HP20x_dev */
  TH02.begin();
  delay(100);
  int humidity =(int)TH02.ReadHumidity();
  SensorValue[HUMI] = humidity;
  return humidity;
}

//get Grove-Moistrue Sensor value
int getMoistrueSensorValue(){
  return (SensorValue[MS] = analogRead(pinMoistrue));
}
//get Grove-Light Sensor value
int getLightSensorValue(){
  return (SensorValue[LIGHT] = analogRead(pinLight));
}
//get Grove-UV Sensor value
int getUVSensorValue(){
  return (SensorValue[UV] = analogRead(pinUV));
}

//Grove PIR Motion Sensor
int getPIRSensorValue(){
  return (SensorValue[PIR] = digitalRead(pinPIR));
}

  
//display Temperature&Humidity Senso value on LCD
void displayTHSensorValue(){
  lcd.clear();
  lcd.print(" Temp&Humidity  ");
  lcd.setCursor(0,1);
  lcd.print("<-");
  char number[16];
  sprintf(number,"%d",getTempSensorValue());
  lcd.setCursor(3,1);
  lcd.print(number);
  lcd.print("C");
  sprintf(number,"%d",getHumiSensorValue());
  lcd.setCursor(9,1);
  lcd.print(number);
  lcd.print("%");
  lcd.setCursor(numCols-2,1);
  lcd.print("->");
}

//display Grove-Moistrue Sensor value on LCD
void displayMoistrueSensorValue(){
  lcd.clear();
  lcd.print("Moistrue Sensor ");
  char number[16];
  int len = sprintf(number,"%d",getMoistrueSensorValue());
  lcd.setCursor(0,1);
  lcd.print("<-");
  lcd.setCursor((numCols-len)/2,1);
  lcd.print(number);
  lcd.setCursor(numCols-2,1);
  lcd.print("->");
}

//display Grove-Light Sensor value on LCD
void displayLightSensorValue(){
  lcd.clear();
  lcd.print("  Light Sensor  ");
  char number[16];
  int len = sprintf(number,"%d",getLightSensorValue());
  lcd.setCursor(0,1);
  lcd.print("<-");
  lcd.setCursor((numCols-len)/2,1);
  lcd.print(number);
  lcd.setCursor(numCols-2,1);
  lcd.print("->");
}

//display Grove-UV Sensor value on LCD
void displayUVSensorValue(){
  lcd.clear();
  lcd.print("   UV Sensor    ");
  char number[16];
  int len = sprintf(number,"%d",getUVSensorValue());
  lcd.setCursor(0,1);
  lcd.print("<-");
  lcd.setCursor((numCols-len)/2,1);
  lcd.print(number);
  lcd.setCursor(numCols-2,1);
  lcd.print("->");
}

//display local ip
void displayLocalIP(){
  IPAddress ip = WiFi.localIP();
  char local_ip[16];
  sprintf(local_ip,"%d.%d.%d.%d",ip[0],ip[1],ip[2],ip[3]);
  local_ip[15]= '\0';
  lcd.clear();
  lcd.print("    Local IP    ");
  lcd.setCursor(0,1);
  lcd.print(local_ip);
}
    

//is button pressed
int isButtonPressed(){
  int state = 0;
  if(digitalRead(pinButton)){
    while(digitalRead(pinButton));
    state = 1;
  }
  return state;
}

void RelayHandle(int val){
  if(val==1) {
    digitalWrite(pinRelay,HIGH);
  }
  else if(val==0){
    digitalWrite(pinRelay,LOW);
  }
}
void BuzzerHandle(int val){
  if(!(val==0 || val==1)) return;
  if(val==1)
    digitalWrite(pinBuzzer,HIGH);
  else if(val==0)
    digitalWrite(pinBuzzer,LOW);
}
void ServoHandle(int val){
  static unsigned long curt = millis();
  if(millis()-curt > 1000){
    myservo.write(val);
    curt = millis();
  }
}

void SleepHandle(int val){
  return;
}  
  
  
void setup() 
{
  Serial.begin(9600);
    // set up the LCD's number of columns and rows:
    lcd.begin(16, 2);    
    Wire.begin();
    WiFi_Init();
      
    pinMode(pinButton,INPUT);
    pinMode(pinRelay,OUTPUT);
    pinMode(pinBuzzer,OUTPUT);
    pinMode(pinEncoder1,INPUT);
    pinMode(pinEncoder2,INPUT);
    myservo.attach(pinServo);
    myservo.write(0);
    
    printSettings();
    
    Timer1.initialize(20000); // set a timer of length 2000 microseconds
    Timer1.attachInterrupt(timerIsr); // attach the service routine here
    attachInterrupt(pinEncoder2,EncoderISR,FALLING);    
}
void EncoderISR(){
    while(!digitalRead(pinEncoder2));
    if(digitalRead(pinEncoder1)==HIGH){
      MenuIndex++;
      if(MenuIndex >= MenuCount) MenuIndex = 0;
    } else {
      MenuIndex--;
      if(MenuIndex < 0) MenuIndex = MenuCount - 1;
    } 
}

//timer interrupt handler
void timerIsr(){
  RequestHandler();
}

// display menu on the LCD screen
void displayMenu(){
  static unsigned long curtime = millis();
  if(millis()-curtime > 1000){
    //noInterrupts();
    switch(MenuIndex){
      case(THSensorIndex):
        displayTHSensorValue();
        break;     
      case(MoistrueSensorIndex):
        displayMoistrueSensorValue();
        break;
      case(UVSensorIndex):
        displayUVSensorValue();
        break;
      case(LightSensorIndex):
        displayLightSensorValue();
        break;
      case(LocalIPIndex):
        displayLocalIP();
        break;
     }
     curtime = millis();
    //interrupts();
  }
}

void TempColorHandle(){
  int temp = getTempSensorValue();
  if(!isBackLightOn){
    lcd.setRGB(0,0,0);
    return;
  }
  if(temp<LOW_TEMP) {
    BLColorRGB[0]=0x00; 
    BLColorRGB[1]=0x00; 
    BLColorRGB[2]=0xFF;
  }
  else if(temp<NOM_TEMP){
    BLColorRGB[0]=0x00;
    BLColorRGB[1]=map(temp,LOW_TEMP,NOM_TEMP-1,0,255);  
    BLColorRGB[2]=map(temp,LOW_TEMP,NOM_TEMP-1,255,0);
  }
  else if(temp<HIGH_TEMP){
    BLColorRGB[0]=map(temp,NOM_TEMP,HIGH_TEMP-1,0,255); 
    BLColorRGB[1]=map(temp,NOM_TEMP,HIGH_TEMP-1,255,0);
    BLColorRGB[2]=0x00;
  }
  else {
    BLColorRGB[0]=0xFF; 
    BLColorRGB[1]=0x00;
    BLColorRGB[2]=0x00;
  }
  lcd.setRGB(BLColorRGB[0],BLColorRGB[1],BLColorRGB[2]);
}  
    
void loop() 
{
  TempColorHandle();
  
  displayMenu();
  
  SerialRequestHandler();
   
  //if button pressed, backlight transforms
  if(isButtonPressed()) isBackLightOn = !isBackLightOn;
  
  //if reconfig WiFi SSID,reconnect.
  if(isSSIDreconfiged==true) {
    status = WL_IDLE_STATUS;
    isSSIDreconfiged = false;
  }
    
  
}

int cmdstrInput(char *str){
  static int index = 0;
  if(Serial.available()){
    char inChar = Serial.read();
    cmdstr[index++]=inChar;
    if(inChar == '\n' || index >= CMDSTR_MAX_LEN){
      cmdstr[index-1]='\0';
      index = 0;
      return 1;
    }
  }
  return 0;
}

//initialize wifi connection 
void WiFi_Init(){
  // check for the presence of the shield:
  if (WiFi.status() == WL_NO_SHIELD) {
    Serial.println("WiFi shield not present"); 
    // don't continue:
    while(true);
  } 

  String fv = WiFi.firmwareVersion();
  if( fv != "1.1.0" )
    Serial.println("Please upgrade the firmware");
}

// print the WiFi connection status using serialport
void printWifiStatus() {
  // print the SSID of the network you're attached to:
  Serial.print("SSID: ");
  Serial.println(WiFi.SSID());

  // print your WiFi shield's IP address:
  IPAddress ip = WiFi.localIP();
  Serial.print("IP Address: ");
  Serial.println(ip);

  // print the received signal strength:
  long rssi = WiFi.RSSI();
  Serial.print("signal strength (RSSI):");
  Serial.print(rssi);
  Serial.println(" dBm");
}

// handl wifi request
void RequestHandler(){
  static unsigned long cur = millis();
  if(status != WL_CONNECTED && *ssid != '\0' && *psw !='\0'){
    if((millis()-cur) > 5000){
      Serial.print("Attempting to connect to SSID: ");
      Serial.println(ssid);
      // Connect to WPA/WPA2 network. Change this line if using open or WEP network:    
      status = WiFi.begin(ssid,psw);
      cur = millis();
    }
  } else if(status==WL_CONNECTED) {
    if(!serverconnected){
      server.begin();
      // you're connected now, so print out the status:
      printWifiStatus();
      serverconnected = 1;
    } else {
      sendpage();
    }
  }
}

// send html to client
void sendpage(){
   // listen for incoming clients
  WiFiClient client = server.available();
  if (client) {
    Serial.println("new client");
    // an http request ends with a blank line
    boolean currentLineIsBlank = true;
    while (client.connected()) {
      if (client.available()) {
        char c = client.read();
        Serial.write(c);
        // if you've gotten to the end of the line (received a newline
        // character) and the line is blank, the http request has ended,
        // so you can send a reply
        if (c == '\n' && currentLineIsBlank) {
          // send a standard http response header
          client.println("HTTP/1.1 200 OK");
          client.println("Content-Type: text/html");
          client.println("Connection: close");  // the connection will be closed after completion of the response
          client.println("Refresh: 2");         // refresh the page automatically every 2 sec
          client.println();
          client.println("<!DOCTYPE HTML>");
          client.println("<html>");
          client.println("<title>Grove Indoor Environment Kit for Edison</title>"); 
          client.println("<font face=\"Microsoft YaHei\" color=\"#0071c5\"/>");
          client.println("<h1 align=\"center\">Grove Indoor Environment Kit for Edison</h1>");
          client.print("
");
          for(int i=0; i < SENSOR_COUNT; i++){
            client.print("<h2 align=\"center\"><big>");
            client.print(SerialVarList1[i]);
            client.print(" = ");
            client.print(SensorValue[i]); 
            client.println("</big></h2>"); 
            //client.print("
");
          }      
          client.println("</html>");
           break;
        }
        if (c == '\n') {
          // you're starting a new line
          currentLineIsBlank = true;
        } else if (c != '\r') {
          // you've gotten a character on the current line
          currentLineIsBlank = false;
        }
      }
    }
    // give the web browser time to receive the data
    delay(1);
    
    // close the connection:
    client.stop();
    Serial.println("client disonnected");
  }
}

Thanks and regards

thanks a lot . its working now

broken again

what is the issue now?

I am using arduino v 1.67 with Intel edison running yocto 2.1
the temp and humidity remains un initialized at -50 and -24 like before
Are there any logs that would be useful in debugging
I will post code and screenshot later

Please download the intel image from the following link

Hi,
The error is during verification ( compilation ) of the code on latest versions of arduino ( 1.6.7 and 1.6.8 )

Please see attached image

Please follow the steps below
1.Delete the existing library from the Arduino IDE 1.6.7
2.Include the new zip file in Arduino IDE 1.6.8.
3.Compile the code in the new IDE.
and Let us know if you have any issues.

Thanks and Regards