Dear techsupport
I run the program “vad_doa.py” with the 6 Mic Circular Array Kit for
Raspberry
Pi (Pi3 Model B+). And the attached file is the log file with the result.
The VAD portion 
of this seems to work but the value returned by mic.get_direction() has no
consistency,
and it seems to cause the program to hang quite often.
I also run the mic_array_dfu, and the result is in the file
“dfu_log”. It shows 
“Could not find/open device”. Is there something wrong?
Can you provide your professional advice for me ? Thanks for your kindly
support.
Hi
Damon,
1. For VAD, the accuracy is 30 degree. you can test it by a record audio and play through cellphone at specific direction.
2. For
mic_array_dfu, it is used for respeaker mic array v1.0, it can not used for the 6 Mic Circular Array Kit for Raspberry.
Thanks
best rgds
Bill
Dear Techsupport
Thanks for your kindly support.
The file ‘vad_doa_log.txt’ is record without any speaking, and the VAD always print ’1’,
Is the function ‘vad.is_speech’ work normally?
Hi Damon,
For the DOA, please use this example to read the DOA.
http://wiki.seeedstudio.com/ReSpeaker_6-Mic_Circular_Array_kit_for_Raspberry_Pi/#librespeaker-aduio-process
For DOA without keyword example, I tested it and it will stuck after running a while. But VAD is 0 when there is no noise and 1 when there is noise. I remove from wiki and check with software team.
---------------------------------------------------------------------
(0, ‘bcm2835 ALSA: - (hw:0,0)’, 0L, 2L)
(1, ‘bcm2835 ALSA: IEC958/HDMI (hw:0,1)’, 0L, 2L)
(2, ‘seeed-8mic-voicecard: - (hw:1,0)’, 8L, 8L)
Use seeed-8mic-voicecard: - (hw:1,0)
11111110011111111111
0
11111111111111111111
100
11111111111111111111
220
11111111111111111111
257
11111111111111111111
319
11111111111000000000
240
000000000000000000000000000000000011111111111111111111111111
280
111100000000000000000000000001111111000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000011111111111000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000011111111000000000000000000000000000000000000000000000000000000000000000000011111111111111
100
11111111111111111111
257
111111100000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000011111111111111111111111111111
257
111111111000000000000000000000000000000000000000000000000000000000000000000000000000011111110000000000000111111111111111
199
11111111111111111111
240
11111111111111111111
  ---------------------------------------------------------------------
Thanks
best rgds
Bill
            Thanks
best rgds
Bill