Dear Techsupport
Thanks for your kindly support.
For DOA without keyword ,If the software have the update version,
please let us know the release link .
We have a project basic on the application.
Best Regards
Damon Lin
???: [email protected] [mailto:[email protected]] ?? seeed_support
???: 2019?3?15? ?? 03:53
???: Damon
??: Re: Question About the Result of vad_doa.py
Hi Damon,
For the DOA, please use this example to read the DOA.
http://wiki.seeedstudio.com/ReSpeaker_6-Mic_Circular_Array_kit_for_Raspberry_Pi/#librespeaker-aduio-process> http://wiki.seeedstudio.com/ReSpeaker_6-Mic_Circular_Array_kit_for_Raspberry_Pi/#librespeaker-aduio-process
For DOA without keyword example, I tested it and it will stuck after running a while. But VAD is 0 when there is no noise and 1 when there is noise. I remove from wiki and check with software team.
(0, ‘bcm2835 ALSA: - (hw:0,0)’, 0L, 2L)
(1, ‘bcm2835 ALSA: IEC958/HDMI (hw:0,1)’, 0L, 2L)
(2, ‘seeed-8mic-voicecard: - (hw:1,0)’, 8L, 8L)
Use seeed-8mic-voicecard: - (hw:1,0)
11111110011111111111
0
11111111111111111111
100
11111111111111111111
220
11111111111111111111
257
11111111111111111111
319
11111111111000000000
240
000000000000000000000000000000000011111111111111111111111111
280
111100000000000000000000000001111111000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000011111111111000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000011111111000000000000000000000000000000000000000000000000000000000000000000011111111111111
100
11111111111111111111
257
111111100000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000011111111111111111111111111111
257
111111111000000000000000000000000000000000000000000000000000000000000000000000000000011111110000000000000111111111111111
199
11111111111111111111
240
11111111111111111111
Thanks
best rgds
Bill
???Helpful? https://seeed.uservoice.com/kudos?kudo=bwJG1YCr%2B7FI%2BY5N4oE0KuX9L46vamLIimkJQWrSPHaukhbUZHtvU64zzwnr6r8FPgczSkUIcbOZI9OsZFAzZQ%3D%3D&tracking_code=60ed602727b6b01177606578d69b530d> Click to give seeed_support thanks!