Quark-n expantion board wifi not working

I am installing the Quantum Mini Linux Development Kit, but the wifi is not working.
When I check the devices in netwrok manager, I don’t see any wifi devices and I can’t connect to them.
I suspect a network chip failure since bluetooth doesn’t work either.

Here is the result of checking the devices with network manager.

pi@Quark-N:~$ nmcli dev
DEVICE TYPE STATE CONNECTION
lo loopback unmanaged –

The system image I’m using is “quark-n-21-1-11.img”.

Any joy getting this solved?