Hi,
wich connector I can use tocconnect to the GPIO Pins of the Quantum Mini Linux Development Kit?
Best Regards
Michael
Hi,
wich connector I can use tocconnect to the GPIO Pins of the Quantum Mini Linux Development Kit?
Best Regards
Michael
I’ve been wondering about this, too. I did a lot of hunting myslelf, but could only figure out that the type of connector is MEC2-DV. These connectors have closed edges, though, so I don’s see how the Atom board can fit as it has the board has the retaining screw for the Quark SoC on one side, and a large SMD capacitor on the other side.
It seems like there was a lot of buzz and info on the board when it was first released two years ago, and then nothing. The schematics released are in a proprietary format (Altium), there’s no device tree, or even a detailed component list (e.g. what TFT is being used, and how can it be addressed?).
And, really, how difficult would it have been to list the specific edge connector type the designer had in mind when he built this thing?