Hi guys!
I working at Pinguino project:
pinguino.cc/
“Pinguino is an easy-to-make Arduino-like board based on 8-bit or 32-bit ©Microchip PIC Microcontrollers with built-in USB module.
Pinguino is also an Integrated Development Environement (IDE) which gives everyone the ability to make easily an application without spending hours learning pragma, configuration bit, command line compiler, etc. The IDE is compatible with Arduino’s Language and Libraries. It’s available on LINUX, WINDOWS and MAC OS X.”
We finishing support for PIC32, and I think Seeedstudio can help us, making boards and accessories.
I have some related posts on my blog: fazzi.eng.br
Another question, how be a partner and reseller of Seeedstudio?