Programming XIAO nrf52840 from nrf52840DK

Hi there,

SO , you can definitely do it, I have a posts or two on it with Pictures and setting used. You can use the NRF_connect Programmer connected to DK as well :+1: SWD from Xiao DEV board to DK and the VDD connection makes it go. :v:

You can tell which is the Target from the NRF_SDK hardware connection will show the Device REV xx check it out works GREAT!

HTH
GL :slight_smile: PJ :v:

2 Likes