I have an RGB LED chainable GROVE and I have downloaded the library with it but I have a problem when I’am doing that:
#include <ChainableLED.h>
ChainableLED leds (6,7,1);
void setup() {
// put your setup code here, to run once:
}
void loop() {
leds.setColorRGB(0,255,0,0);
delay(1000);
leds.setColorRGB(0,0,0,0);
delay(1000);
}
With just this little program, the color of LED stays the same and I don’t know why! There is no change
If someone can help me to understand that. Thanks a lot
I must say that programs that I’ve downloaded on the site are working but mine not!
Hi there~
You missed the leds.init() inside of setup(). thanks.
[code]#include <ChainableLED.h>
ChainableLED leds (6,7,1);
void setup() {
leds.init();
}
void loop() {
leds.setColorRGB(0,255,0,0);
delay(1000);
leds.setColorRGB(0,0,0,0);
delay(1000);
}[/code]
you seem to be wright!
I believe that it was not necessary to do that because on the program in the tuto the function was not written.
Thanks!