I have purchased a Wio LTE Cat M1/NB-IoT Tracker and finally been able to connect to it, but I need to change the APN it connects to and provide a username and password.  I have tried all AT commands that look like it should work but I suspect it needs a correct sequence of commands.  I now the SIM card works fine because I have tested it in another Cat M1 device.  
Can you please provide the sequence of AT commands to change the APN and add a username and password to connect to the Private APN?
Hi, please refer to below. fore more info, please refer to 13.1.3    Parameter definition of <LINK_TEXT text=“https://www.u-blox.com/sites/default/fi … 787%29.pdf”>https://www.u-blox.com/sites/default/files/SARA-R4-SARA-N4_ATCommands_(UBX-17003787).pdf</LINK_TEXT>
An example for the usage of  is:
AT+CGDCONT=1,“IP”,“CHAP:internet.t-d1.de”
thanks
Bill
Hello,
I have figured out what to do to make it work.  The AT Command manual has some errors in it.
The example in the AT Command Manual doesn’t work.
AT+CGDCONT=1,“IP”,“PAP:telstra.corp”
+CME ERROR: operation not supported
If I change it to the following, it works.
AT+CGDCONT=1,“IP”,“telstra.corp”
OK
Changing the APN now works, but entering the username and password is now the problem.
I have tried the following AT command but doesn’t register to the new APN.
AT+UAUTHREQ=1,1,“user”,“pass”
If I swap the username and password around, it works.
AT+UAUTHREQ=1,1,“pass”,“user”
Below is the list of commands I used to get it to register to my Private APN:
AT+CFUN=4
AT+CGDCONT=1,“IP”,“APN”
AT+UAUTHREQ=1,1,“password”,“username”
AT+CFUN=1
Hi, thanks for keeping us posted. 
Bill