According to the nRF54LM20A datasheet, the operating temperature range is -40 to 85 degrees Celsius.
With a simple LoRa based battery operated “-40°C freezer temperature project”, I’d probably go for the Seeed Wio-E5 and flash it (over SWD ->STLink/JLink) using the appropriate (STM32 or Arduino) code and libs.
Use a Lithium Manganese Dioxide battery and 1.8V LDO. Add any essential sensors using I2C.
Battery → LDO → Wio-E5 ↔ Sensors
Hi there,
Great
my guy.
-40
GL
PJ ![]()
Hi there,
So completely ignoring the actual hardware the OP is trying to work through and essentially replying, “Just throw all that out, buy a Wio-E5, flash it with an ST-Link, and build a totally different project.” It doesn’t answer actual confusion about the LDO dropout, peak currents, or RadioLib internals.
SO staying on point , I know it’s a FAT topic for some. but to your question about the RadioLib LDO vs. DC-DC setting:
-
RadioLib’s Setting is purely for the internal SX1262 core: It controls the transceiver’s internal step-down regulator (pin
REG_MODEpowering the RF core from VDD), not the board’s power rail. -
DC-DC is the right choice: Setting
setRegulatorLDO()burns extra current as heat. SettingsetRegulatorDCDC()(which the Seeed LoRa expansion/breakout boards wire for) drops the RX/TX current draw significantly—roughly cutting receive current in half (~4.6 mA vs ~8.4 mA) and shaving crucial milliamps off peak TX.
HTH
GL
PJ ![]()
You know " No Pain NO Gain! ![]()
Or
Off into the Weeds you Go! ![]()
Further to this Simple Single CPU coin cell battery based, low power option using a Seeed Wio-E5, if I wanted to test and prove the “theory” with minimal expertise or complexity, I’d use a Seeed Grove Wio-E5 module.
To achieve lower battery voltage and power consumption, I’d replace the AP7333-33SRG LDO with a Torex XC6206P182MR-G (which matches the pinout). I’d also add 2x 47uF Tantalum-Polymer Capacitors for power support (Coin Cells and LDO).
Total cost for Wio, LDO and Caps ~USD20.
Hi there,
So I looked a little further..
For a standard domestic freezer running at -18°C to -20°C, the board will run, but you are right on the edge of Seeed’s official rating. The distinction between Nordic and Seeed comes down to the rest of the bill-of-materials:
The Nordic vs. Seeed Difference
-
The Nordic SoC: Nordic rates bare silicon (both nRF52840 and nRF54L series) for full industrial range (-40°C to +105°C). The chip itself will function without issue down past -30°C.
-
The XIAO Board BOM: Seeed derates the overall module to -20°C to 70°C because of ancillary parts: the external flash memory (PY25Q64), the low-cost 32.768 kHz / 32 MHz crystal oscillators, passive ceramic caps, and the onboard PMIC/LDO. Standard commercial crystals can drift or struggle to start oscillating when pushed below -20°C.
HTH
GL
PJ 
I see , the recomends for the environment, but what is the situation?
Recommended Setup for a Freezer Node
-
Power Source: Use Energizer Ultimate Lithium (L91 AA/AAA) or spiral-wound industrial lithium cells. Lithium iron disulfide ($Li\text{-}FeS_2$) is explicitly rated down to -40°C and does not suffer the instant voltage collapse that LiPo or bobbin-cell chemistries experience below freezing.
-
Antenna: Keep the radio outside the box with a flat wire probe (like a DS18B20 or thermistor) running past the door gasket, or route an external antenna pigtail out of the seal if the whole node must stay inside.
-
?
LOL,
I want to try this Now…Jezz
regulator has a dropout voltage of ~200–300 mV, meaning the battery input rail must sit at > 3.5V–3.6V
I cannot find it anywhere. I am missing some parts here:
Xiao nRF52480 flash internal, no sensors, no mic.
VBAT → LP0404N3T5G → LDO SGM2040-3.3 ±-> VDD nRF52840
LDO ±-> VCC Wio SX1262
VDD input directly into the nRF52840 with just a few capacitors.
Output is from nRF52840 - capacitors & resistors to the antenna, etc
SGM2040 - Low Dropout CMOS Voltage Regulator
VIN operating range: 1.7-7.5V
VOUT: 3.3V (for SGM2040-3.3)
IOUT: 250mA max
IQ (self-consumption): 1µA typ, 1.5µA max
VDROP: 70-90mV @100mA & 25°C
If VIN >= VOUT(NOM) + VDROP
→ VOUT is regulated
If VIN < VOUT(NOM) + VDROP
→ regulator enters dropout mode
→ VOUT is unregulated
→ regulator does not boost voltage
→ VOUT ≈ VIN - VDROP
Hi there Johann,
Spot on catch regarding the LDO specs! That clears up the confusion nicely.
You’ve got the exact right breakdown on how that power rail behaves:
-
Low Dropout Advantage: With the SGM2040’s typical dropout at only 70–90 mV @ 100 mA, you get considerably more headroom before the rail starts to dip compared to older-style regulators.
-
Dropout Mode Behavior: Once VIN < VOUT(NOM) + VDROP, the regulator simply enters dropout mode rather than cutting power. VOUT tracks roughly at VIN - VDROP without boosting, which works out well here since the nRF52840’s internal supply range is comfortable operating well below a strict 3.3V.
Great detective work pulling the actual component values from the schematic—makes a big difference when calculating real-world runtime on primary cells!
HTH
GL
PJ ![]()
What I understand, the theoretical part of it, with a lower LDO, you just trade power for heat. Since nRF52840 has already a regulator, maybe it is better to feed 3V battery directly into 3.3V rail? But in this case you rely on the battery quality.
Yes, that will work for your battery voltage (ie 3V). It does depend on your battery, as well as your required device “longevity” before battery failure.
Since the devices you are looking at (including the STM32WLE5JC in the Grove Wio-E5), have internal DC-DC converters, an external LDO isn’t really necessary if the battery voltage is within their range (so your 3V cell is fine).
Finally, I would still add some bulk capacitance to support the battery during transmission.
If you have a suitable 3V battery that works at the -40°C temperature, then the XIAO NRF52840/SX1262 solution should be fine ![]()