Possible bug on Grove Pi

Hi



I have been working with the Grove Pi for only some days, but have worked with the RPi for about a year and have done a few projects.

I really like the Grove Pi as I can do things better and faster.



So I have been building a setup to measure air quality using the sensors for Humidity&Temperature and Dust.

I was trying to add the light and sound sensors, but eventhough I get output - its the same.

Somehow I think the data from the sound sensor is copied to the light sensor.

First I setup the light sensor to A2 and sound to A0. Same data was collected.

Then I moved the lightsensor to A1, but didnt update the code to reflect it. Same data was collected.

Then I updated the code. Same data was collected.



So what I conclude from this is that the data from the soundsensor is applied to the lightsensor. Either in code, firmware or hardware.



This is my code:
[code]from future import print_function
import paho.mqtt.publish as publish
import psutil
import string
import random
import time
import grovepi
import atexit
from grove_rgb_lcd import *
from grovepi import *

#Setting up sensors
atexit.register(grovepi.dust_sensor_dis)
sensor = 7 #D7
LightSensor = 1 #A2
SoundSensor = 0 #A0
LED_green = 4 #D4
LED_red = 3 #D3
pinMode(LED_green,“OUTPUT”)
pinMode(LED_red,“OUTPUT”)
grovepi.dust_sensor_en()
last_sound=0

#Setting up data to write data to Thingspeak
string.alphanum=‘1234567890avcdefghijklmnopqrstuvwxyzxABCDEFGHIJKLMNOPQRSTUVWXYZ’
channelID = “XXXXXXXXX”
writeAPIKey = “XXXXXXXXX”
mqttHost = “mqtt.thingspeak.com”
mqttUsername = “TSMQTTRpiDemo”
mqttAPIKey =“XXXXXXXXX”
tTransport = “websockets”
tPort = 80
topic = “channels/” + channelID + “/publish/” + writeAPIKey

while True:
try:

            #Set green operation
            digitalWrite(LED_green,1)
            digitalWrite(LED_red,0)

            #Gather data from sensors
            [new_val,lowpulseoccupancy] = grovepi.dustSensorRead()
            [temp,hum] = grovepi.dht(sensor,0)
            light_intensity = grovepi.analogRead(LightSensor)
            sound_level = grovepi.analogRead(SoundSensor)
            
            if sound_level > 0:
                    last_sound=sound_level

            #Prep connection to Thingspeak
            clientID=''
            # Create a random clientID.
            for x in range(1,16):
                    clientID+=random.choice(string.alphanum)

            #To avoid posting empty data as "0" from the dust sensor. New_val means there is new data
            if new_val:
            
                    #Show data
                    print ("Temp =", temp, "C & Humidity =", hum,"% & Dust consentrantion =",lowpulseoccupancy," & Light =",light_intensity," & Sound =",last_sound)

                    #Prepare data for use on LCD & Thingspeak
                    t = str(temp)
                    h = str(hum)
                    d = str(lowpulseoccupancy)
                    l = str(light_intensity)
                    s = str(last_sound)

                    # build the payload string for Thingspeak
                    payload = "field1=" + t + "&field2=" + h + "&field3=" + d + "&field4=" + l + "&field5=" + s

                    # attempt to publish data to the topic on Teamspeak.
                    try:
                            publish.single(topic, payload, hostname=mqttHost, transport=tTransport, port=tPort,auth={'username':mqttUsername,'password':mqttAPIKey})
                            print (" Published to Teamspeak to host: " , mqttHost , " clientID= " , clientID)

                    except (KeyboardInterrupt):
                            break
                    except:
                            print ("There was an error while publishing the data.")
                            digitalWrite(LED_green,0)
                            digitalWrite(LED_red,1)

                    #Set LCD color
                    setRGB(0,128,64)
                    setRGB(0,0,255)
                    #Print on LCD
                    setText("T:" + t + "C" + " H:" + h + "%" + " Dust:" + d + "psc/L")

            #Wait 5 seconds
            time.sleep(5)
            
    except (IOError,TypeError) as e:
            print("Error")
            digitalWrite(LED_green,0)
            digitalWrite(LED_red,1)<e>[/code]</e></CODE>

I have checked it several times, but I cant find the fault in the code itself. Can you find fault?

I have tested a bit more and I get data from the sound sensor, even when its not connected.



If I disable code for the temperature and humidity, then it works for the light sensor…its really strange!

I made a separate script to test the light sensor and that works…



Any points to errors on my code?

Hi there

We are checking your questions. We will reply to you as soon as possible after the investigation.

Hi there

Please submit your question here. https://forum.dexterindustries.com/