Performance Jetson Orin NX 16GB

Hi everyone,

I’m working with the Orin NX 16GB and running YOLOv8 for object detection tasks. Initially, after flashing a fresh system, I ran some benchmarks and got the somewhat the expected performance. However, after installing Redis and RabbitMQ, I noticed a significant drop in performance. I conducted another round of benchmarks after downloading these services, and the performance had worsened drastically.

Here’s what I’ve tried so far:

  • Disabled both Redis and RabbitMQ, but this hasn’t improved the performance.
  • Verified that no other intensive processes are running.
  • Fresh installation of Jetson software

I have followed the following tutorials:
NVIDIA Jetson - Ultralytics YOLO Docs
Deploy YOLOv8 with TensorRT | Seeed Studio Wiki

Has anyone else experienced similar issues with Redis/RabbitMQ or other services impacting the Orin NX performance? Any suggestions for troubleshooting or fixing this problem would be greatly appreciated!

Thanks in advance for your help.

Best regards,
Koen

The data:

Format Status Size (MB) mAP50-95(B) Inference Time (ms/im) FPS
PyTorch ✅ 6.2 0.6381 107.54 9.30
TorchScript ✅ 12.4 0.6117 14.26 70.10
ONNX ✅ 12.2 0.6117 21.74 45.99
OpenVINO ❌ 0.0 0.0000 0.00 0.00
TensorRT ✅ 16.1 0.6092 7.99 125.15
CoreML ❌ 0.0 0.0000 0.00 0.00
TensorFlow SavedModel ❌ 0.0 0.0000 0.00 0.00
TensorFlow GraphDef ❌ 0.0 0.0000 0.00 0.00
TensorFlow Lite ❌ 0.0 0.0000 0.00 0.00
TensorFlow Edge TPU ❌ 0.0 0.0000 0.00 0.00
TensorFlow.js ❌ 0.0 0.0000 0.00 0.00
PaddlePaddle ✅ 24.4 0.6092 611.20 1.64
NCNN ✅ 12.2 0.6034 47.95 20.85

and after installation of redis and rabbitmq

Format Status Size (MB) mAP50-95(B) Inference Time (ms/im) FPS
PyTorch ✅ 6.2 0.6381 106.69 9.37
TorchScript ✅ 12.4 0.6117 14.24 70.21
ONNX ✅ 12.2 0.6117 24.29 41.18
OpenVINO ❌ 0.0 0.0000 0.00 0.00
TensorRT ✅ 15.8 0.6091 14.21 70.38
CoreML ❌ 0.0 0.0000 0.00 0.00
TensorFlow SavedModel ❌ 0.0 0.0000 0.00 0.00
TensorFlow GraphDef ❌ 0.0 0.0000 0.00 0.00
TensorFlow Lite ❌ 0.0 0.0000 0.00 0.00
TensorFlow Edge TPU ❌ 0.0 0.0000 0.00 0.00
TensorFlow.js ❌ 0.0 0.0000 0.00 0.00
PaddlePaddle ✅ 24.4 0.6092 595.86 1.68
NCNN ✅ 12.2 0.6034 35.49 28.18