As per the document provided by SeedStudio WiKi, I tried to flash OrinNX after installing NVMe 256G SSD on A603 carrier board.
wiki.seeedstudio.com

A603 Carrier Board
I overwrote it with the driver for A603 provided by SeedStudio and proceeded with Flash with the command below.
sudo ./tools/kernel_flash/l4t_initrd_flash.sh --external-device nvme0n1p1 -c tools/kernel_flash/flash_l4t_external.xml -p “-c bootloader/t186ref/cfg/flash_t234_qspi.xml” --showlogs --network usb0 p3509-a02 +p3767-0000 internal
However, I get an error that says Return Value 4.
Error Log
Attached is the serial console log.
Serial Console Log
If i execute the above Flash command again without rebooting OrinNX,
A Return Value 8 error appears.
Flash Error Log
The serial console only shows the message below.
C> XUSBF: comp_code went out of sequence. Expected 1 insted of 223.
What could be the problem?
You may need to answer a few questions so that I can better solve your problem:
-
Do you enter recovery mode by adding the jumper? If you did, send a photo of lsusb command.
-
which jetpack version do you flashed?
-
please make sure the micro-usb cable you are using supports data
-
which version of Ubuntu do you use on your PC
- Connect the jumper to enter recovery mode.
Below is the lsusb command output.
(base) hexafactory@hexafactory-1804:~$ lsusb
Bus 004 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub
Bus 001 Device 003: ID 046d:c534 Logitech, Inc. Unifying Receiver
Bus 001 Device 006: ID 0955:7323 NVidia Corp.
Bus 001 Device 004: ID 8087:0026 Intel Corp.
Bus 001 Device 002: ID 067b:2303 Prolific Technology, Inc. PL2303 Serial Port
Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub
-
The jetpack version uses 5.1.1.
-
This is a micro-usb cable that supports four data.
I’ve tried using a different cable and it’s the same.
-
ubuntu 18.04 / intel
(base) hexafactory@hexafactory-1804:~$ uname -a
Linux hexafactory-1804 5.4.0-150-generic #167~18.04.1-Ubuntu SMP Wed May 24 00:51:42 UTC 2023 x86_64 x86_64 x86_64 GNU/Linux
I found that this problem is caused by the WiFi module (Intel) installed in the M.2 E port of the SeedStudio A603 Carrier board when flashing.
When flashing, do not install anything except NVMe SSD, and install M.2 e WiFi module after installation and booting is completed.
problem solving!