On ODYSSEY - X86J4125, I had wiped out the eMMC drive and reformatted the drive as NTFS.
Prepared an NTFS USB drive, extracted the SEEED Windows OS files into the USB root directory, (taken out of the main folder SD-JX-CJ41G-M-101-H and deleting the empty folder SD-JX-CJ41G-M-101-H.
From the instructions here:
Seeed Studio: Re-Installing the Original Windows
However, when I attempt to boot the USB drive, the UEFI option within the boot options, Windows loads briefly, to install with the logo, then crashes, or errors out with a missing: file \windows\system3boowinload.efi error.
Do I need to reinstall the BIOS for Windows Boot Manager to show up in BIOS instead of just ‘Windows Restore’ which errors out on boot?
Or is there an other workaround this issue?
Thanx