X0X0X0
1
Board Information
Product Version: ODYSSEY-X86J41X5
BIOS Version: SD-BS-CJ41G-Hb
Build Date and Time: 11/02/2021 17:30:02
Access Level: Administrator
Platform firmware Information
TXE FW: 4.0.15.1303
EC Version: 02.0E.OB(PO)
GOP: 13.0.1018
Within BIOS settings > Boot:
Boot Option Priorities
I do have [debian] listed twice.
How do I remove the duplicate, or the second [debian] option from BIOS?
Thank you
BIOS Boot Option
X0X0X0
2
Wiping out the MMC drive did resolve the issue.
I attempted to utilize Windows DISKPART cmd and CMD to delete the extra ‘debian’, or any other ‘debian’ boot options:
In summa, attempt such steps within Windows CMD that is executed as “Run as Administrator”
diskpart
DISKPART>list disk
....
DISKPART>sel disk 0
DISKPART>list vol
....
DISKPART>sel vol 3
DISKPART>assign letter=G:
After this, I had to close the CMD window and reopen (or just exit from DISKPART)
> cd /d g:
>dir /B
If you find efi folder then change directory to:
>cd /d efi
If needed, delete the directory:
>rmdir /S ubuntu
This is a rough outline of what is required to delete an extra boot option via Windows OS terminal.