Odyssey X86 - Defective FAN

Maybe the sensors have a bit late compare with the system sensor.

@rgl, @solidus1983 (+ others) – did any of you upgrade to the most recent firmware (and EC) versions – and if so did the changes have an impact on how the fan is operating?
(The most recent at the time of writing appears to be SD-BS-CJ41G-300-101-F. https://files.seeedstudio.com/wiki/ODYSSEY-X86J4105864/Documents/SD-BS-CJ41G-300-101-F.zip)

I am also experiencing this issue; fan does not work at all when in “Always On” mode, even when all sensors reach over 90C (194F), 5 degrees centigrade below critical point (tested with MPrime). When set to “Normal” or “Positive”, it only creates a very annoying ticking/scratching sound, and the fan is constantly “revving” up and down, without doing any real work.

Since there have been reports of firmware upgrades bricking the Odyssey, it would be extremely helpful to know for sure whether this is actually a software issue or hardware-related before attempting a fix.

Thanks for any input. :+1:

@milasx (who I also notice is using sensors on Linux) + @komorebi: did any of you try the firmware update fix for the defective (non-spinning) fan-issue?

Yes and the fan seems more responsive to temperature changes. Unfortunately there is no way to monitor the speed of the fan so we cannot be sure but it seems to spin more than before and it is not stuck.

Thanks for confirming, @milasx. My main issue was that the fan was either completely switched off (when, ironically, it was in “Always On” mode), or did its constant “revving-up” thing while in “Normal” or “Positive”. I’m normally not a fan of fan noise (pun intended), but the scratching and ticking sound really became bothersome, even when it was in the other side of the room.

I’ll try a firmware upgrade, but obviously wanted to make sure if there were adverse effects in doing this beforehand, since some users reported that the Odyssey was left in an unbootable state after doing so (which is – shall we say – suboptimal)

btw. did you also remove the CMOS battery as the guide suggested (presumably to set it back to factory defaults)?

Be easy to upgrade the firmeare. The EC first, then BIOS. Upgrade the BIOS may take severial miniutes, donot remove the power or force restart the machine unless you see the boot logo showed in the screen.

@Drag0nFly I had the same problem as you say and the update fixed it. I did not remove the CMOS battery. I followed the instructions as per post from @Bruce.Qin.

Fingers crossed for you!

Ignore the post about the sha256sums, I see now that they are based on the actual zip file, not the BIOS files (which is more common practice).

It’s probably a good idea to mention upgrading the EC firmware prior to the BIOS on the Wiki though, based on the comments above, as it sounds like a critical step.

Waitting your good news.

Finally did the EC + BIOS upgrade – happy to report that both went without a hitch. :slight_smile: Now both my Odyssey-based systems are running the same BIOS: (I have one J4105 + the new J4125)

dmesg -T|egrep ‘Celeron|SD-BS’
[Fri May 7 20:51:11 2021] DMI: Default string ODYSSEY-X86J4125/ODYSSEY-X86J41X5, BIOS SD-BS-CJ41G-300-101-F 04/08/2021
[Fri May 7 20:51:12 2021] smpboot: CPU0: Intel® Celeron® J4105 CPU @ 1.50GHz (family: 0x6, model: 0x7a, stepping: 0x1)

[Tue May 4 20:25:40 2021] DMI: Default string ODYSSEY-X86J4125/ODYSSEY-X86J41X5, BIOS SD-BS-CJ41G-300-101-F 04/09/2021
[Tue May 4 20:25:41 2021] smpboot: CPU0: Intel® Celeron® J4125 CPU @ 2.00GHz (family: 0x6, model: 0x7a, stepping: 0x8)

Initially thought the EC hadn’t changed, as I could not identify its version in the BIOS (completely different from the filename). But I can confirm that the fan behaves correctly now, in that “Always On” does actually mean what it says, and Normal has the fan running (in a low-rpm, so it is very silent, basically inaudible unless you put your ear next to it. Good stuff.)

For the upgrade I did a complete power drain for both EC & BIOS. EC went very fast. The BIOS took longer than expected (before the reboot). After it finished I turned it off, unplugged the DC and let the voltage drain. I did not remove the CMOS battery connector for either EC or BIOS.

The subsequent bootup took around 3-4 minutes, with 2 reboots in between.

btw. – it took some time to realize that the EFI System Shell for some reason did not support an exfat filesystem, which was a little strange (don’t usually have older FAT-based filesystems lying around, so a stick had to be formatted for it). For the record - many EFI Shells also support Linux filesystems now (ext4/ext3) as well, and it would be nice if Seeed supported this also, considering how many users buy it in order to run a Linux variant or pfSense etc.

Also did some testing with memtest86+ and MPrime (Prime95 for the W*n crowd) using its torture test (#1, small FFTs). It’s the most CPU and heat-intensive app that I know of.

Where the previous BIOS managed to get it up to 95C (203F) – where it had to be manually terminated for safety reasons, the new BIOS (in ‘Normal’ setting) hovers around 71-73C (157-163F); all while running completely silent.

So for my part at least the issue is resolved – kudos to the Seeed techs for fixing the fan issue. It would as I mentioned be nice if the EFI shell supported more filesystems, so feel free to take that as a suggestion for a future BIOS version.

Glad to hear that. Exfat file system not support yet. I think you are the first batch recieved the new CPU. :grinning:

So ya That’s a thing. Been using this Computer for a few months and Never noticed the fan issue. It’s been winter and cold. I didn’t push this computer very hard so I never heard the ticking till it got warm out.

I Guess I could do this BIOS and EC update.
I do wish we could have been Notified about it.
Maybe it doesn’t matter it’s just for completeness.

If I brick this thing I’ll be pretty upset. So Seeed need to make sure there doing the right thing for there customers. I think this is a great product don’t let us down now.

Hope you all get yours working 100% and would love to see what your all doing with theres.

Do you work for Seeed. Thanks

We don’t recommand to update the BIOS if it worked for you.
Yes, I am hardware engineer of Seeed, look around to hear your voice from time to time.

Gents,

I’ve done both firmware and EC updates to my X86J4105 but the fan still does the annoying ticking sound in “Normal” mode.
“Always on” does what it says but it’s loud, and “disabled” switches the fan off completely.
But what I need it the Normal mode to work. Any ideas?

Currently my odyssey has the latest
BIOS firmware SD-BS-CJ41G-300-101-H (wiki release date 16/08/2021) and
EC firmware SD-EC-CJ41G-M-101-Q (wiki release date 10/12/2021) (which shows as “EC version 02.0D.09” in the BIOS screen)

Update: It finally works. I had to redo the BIOS update and religiously follow the steps 4 & 5:

Step 4 - Reboot

  • When the BIOS is upgraded, press the ON/OFF button, and you should see the blue light goes off.
  • Unplug the DC power jack and RTC battery from the ODYSSEY-X86.
  • Wait a couple of minutes
  • Plug the RTC battery and DC power jack back to the ODYSSEY-X86.
  • Press the ON/OFF button and wait patiently. You should see the blue light goes on.

Step 5 - Wait Patiently

Please wait patiently and DO NOT unplug power (or the hardware) to corrupt the updating process. The process will take 6 ~ 8 minutes, feel free for a coffee break!