ODYSSEY STM32MP157C ARM Trusted Firmware support?

@166291

Thanks for the inputs.
Now i tried following things ->
Your kernel + Your Custome ATF (v2.2-LS + patch from @ekorre ) + Seeeed’s U-boot

ERROR:   stm32_sdmmc2_init: DT Error
PANIC at PC : 0x2ffd91e1

I haven’t changed any settings in make menuconfig just kept it stm32mp157c-dk2 all the way.
Except in case of kernel where i have kept it as : stm32mp157c-odyssey.dts

Update : Tried with 2.4-LS branch , getting the same kernel panic. Also few changes in the headers files were missing incorporated that , but still looking at the kernel panic.

�NOTICE:  CPU: STM32MP157CAC Rev.B
NOTICE:  Model: STMicroelectronics STM32MP157C-DK2 Discovery Board
ERROR:   stm32_sdmmc2_mmc_init: DT error
ERROR:   SDMMC1 init failed
PANIC at PC : 0x2ffd52d1