I have a ODB II RF Dev Kit that I’ve had for a bit, but haven’t been able to get it to seem to power up when connected to my vehicle (2020 Honda Ridgeline). Today I finally had time to try to power it up via the place where the header is shown in the picture (the board I have doesn’t have a header installed, but I’ll be adding one this evening).
Supplying 3.3V and Ground shows a blue light on the radio part of the board. The other thing I’ve noticed is that not all the pins are soldered from the ODB-II connector to the board. I’ve attached two photos (top and bottom view) that show what is soldered.
The other odd thing I’ve seen is that two of the pins in the OBD-II connector stick noticeably further out than the other pins. Could this be causing a problem seating the connector to the car? If so, it’s a defect that has been here since I got the board…
Would like to be able to get this working… any pointers would be appreciated.
Earl