Having become somewhat familiar with using Zephyr+NCS, I wrote a simple project for practice to send and receive data bidirectionally between the nRF54L15 Peripheral and Central. I hope it proves useful to anyone interested.
Both the Peripheral and Central send and receive 16 bytes of data (timestamp, battery voltage, RSSI, and each other’s random number) to each other every second. The transmitted random number is received with a periodic delay, allowing for verification. When running on battery power, set CONFIG_SERIAL=n. The transmit power is set to 8dBm by specifying CONFIG_BT_CTLR_TX_PWR_PLUS_8=y, but this can be changed and verified by observing changes in the RSSI value.
This might be specific to my environment, but a recurring issue is that flashing via USB using “west flash” often fails, or if it does flash but it frequently causes a FAULT. Performing a “factory_reset” does not resolve this. As a workaround, I’m now flashing using J-Link, which is stable.
My impression is that with Arduino and nRF54820, I could have built the same project much faster. Even though it was my first time, using nRF54L15 with the complex Zephyr+NCS stack took nearly a month. Not being able to reuse assets written for Arduino made it very inefficient.
The project and hex files are located in the folder below.
BLE_bidirectional.zip (901.7 KB)
1 Like
Hi there,
Awesome, Sample my Guy
I’m waiting on some external Antenna’s to arrive for a range test. I would agree, There is something off on the West Flashing tech.
Users YMMV, The JLink is Rock Solid the more I use it the more I like the Whole package, RTT Viewer and SDK and DEV board.
I too switched to the JLink runner and haven’t had one go south yet. WIth the West Flash Tech , seemed like every 3rd or 4th flash the part would FAULT and JLink fixed them every time. I had the same as you outcomes with the (restore Script) just did NOT work reliably.
I think it’s a speed issue with the Samd11 front end.
and or the config file may need some additional fine tuning.
The 54 is a nice MCU though and I think with the MCUBoot and the DFU capabilities will serve users well who need that. More maturity on the SDK will only get better so I’M confident the Juice will be worth the Squeeze

the Deep_throat
is whispering a 54LM20 Xiao could be in the works with built in High speed USB and High Speed SPI, 2 Meg NVM and 512k RAM so that will be a catapult to Anything already built or understood. This is I see the advantage, You can just build for a different targets and the APP can be coded to be MCU agnostic and expandable Ram memory and Flash gives instant boost and features like crashproof DFU. Newer Soft devices are expected also for the 54 Series. Supporting some Advanced BLE features.
More RAW HorsePower(2x) @Less than (half) current consumption, Battery Status readable, BLE 6.0 with Channel Sounding. Definitely going in the right direction.
Keep them coming. 
GL
PJ