Is it possible to enter deep sleep, but keep track of the time?
sd_power_system_off();
I’m using the arduino framework where you can get millis() since start-up. Is there a way to get millis the device was shut down for without any additional hardware like an RTC?
Hi there,
I would use RTC for most reliable and accurate* But others have used the SAMD-21
like in this link.https://forum.arduino.cc/t/low-power-sleep-how-to-keep-track-of-time/1091051
LowPower.deepSleep(milliseconds);
HTH
GL PJ
Tobias
June 19, 2023, 2:58pm
3
Can the Nrf52 XIAO wake up from deep sleep at specific time intervals? If so, how is this achieved?
Hello,
Have a LQQK at this, The Xiao Nija Msfujino’s excellent work and research on it
In a project to periodically write data to an on-board flash memory, I used System_ON_Sleep to reduce the standby current to 1/60th of its default value.
As a practical example, described here is that XIAO wakes up from System_ON_Sleep every hour and records temperature, humidity, and barometric pressure data measured by the BME280 into 2MB of > on-board flash memory.Measures to reduce current consumption include…
nRF52840: REG 1 in DC/DC mode, System_ON_Sleep mode, and wake-up with RTC inter…
HTH
GL