Hi,
I have been attempting to write and store data using the nRF52840 and XIAO round display. To start, I wanted to try out these example programs and then integrate the BLE program into other program. However, this example program itself is not providing the expected output when connected to my Bluefruit Connect application.
Pls find the screenshots ![]()
Hi there,
So how is this connected?
can you show a picture?
the LED are you just trying to turn it on and off?
LMK
GL
PJ
This is the code:
/*********************************************************************
This is an example for our nRF52 based Bluefruit LE modules
Pick one up today in the adafruit shop!
Adafruit invests time and resources providing this open source code,
please support Adafruit and open-source hardware by purchasing
products from Adafruit!
MIT license, check LICENSE for more information
All text above, and the splash screen below must be included in
any redistribution
*********************************************************************/
// This sketch is intended to be used with the NeoPixel control
// surface in Adafruit's Bluefruit LE Connect mobile application.
//
// - Compile and flash this sketch to the nRF52 Feather
// - Open the Bluefruit LE Connect app
// - Switch to the NeoPixel utility
// - Click the 'connect' button to establish a connection and
// send the meta-data about the pixel layout
// - Use the NeoPixel utility to update the pixels on your device
/* NOTE: This sketch required at least version 1.1.0 of Adafruit_Neopixel !!! */
#include <Arduino.h>
#include <Adafruit_NeoPixel.h>
#include <bluefruit.h>
#define NEOPIXEL_VERSION_STRING "Neopixel v2.0"
/* Pin used to drive the NeoPixels */
#if defined ARDUINO_NRF52840_CIRCUITPLAY || defined ARDUINO_NRF52840_FEATHER
#define PIN PIN_NEOPIXEL
#elif defined ARDUINO_NRF52832_FEATHER
#define PIN 30
#else
#define PIN 6
#endif
#define MAXCOMPONENTS 4
uint8_t *pixelBuffer = NULL;
uint8_t width = 0;
uint8_t height = 0;
uint8_t stride;
uint8_t componentsValue;
bool is400Hz;
uint8_t components = 3; // only 3 and 4 are valid values
Adafruit_NeoPixel neopixel = Adafruit_NeoPixel();
// BLE Service
BLEDfu bledfu;
BLEDis bledis;
BLEUart bleuart;
void setup()
{
Serial.begin(115200);
while ( !Serial ) delay(10); // for nrf52840 with native usb
Serial.println("Adafruit Bluefruit Neopixel Test");
Serial.println("--------------------------------");
Serial.println();
Serial.println("Please connect using the Bluefruit Connect LE application");
// Config Neopixels
neopixel.begin();
// Init Bluefruit
Bluefruit.begin();
Bluefruit.setTxPower(4); // Check bluefruit.h for supported values
Bluefruit.Periph.setConnectCallback(connect_callback);
// To be consistent OTA DFU should be added first if it exists
bledfu.begin();
// Configure and Start Device Information Service
bledis.setManufacturer("Adafruit Industries");
bledis.setModel("Bluefruit Feather52");
bledis.begin();
// Configure and start BLE UART service
bleuart.begin();
// Set up and start advertising
startAdv();
}
void startAdv(void)
{
// Advertising packet
Bluefruit.Advertising.addFlags(BLE_GAP_ADV_FLAGS_LE_ONLY_GENERAL_DISC_MODE);
Bluefruit.Advertising.addTxPower();
// Include bleuart 128-bit uuid
Bluefruit.Advertising.addService(bleuart);
// Secondary Scan Response packet (optional)
// Since there is no room for 'Name' in Advertising packet
Bluefruit.ScanResponse.addName();
/* Start Advertising
* - Enable auto advertising if disconnected
* - Interval: fast mode = 20 ms, slow mode = 152.5 ms
* - Timeout for fast mode is 30 seconds
* - Start(timeout) with timeout = 0 will advertise forever (until connected)
*
* For recommended advertising interval
* https://developer.apple.com/library/content/qa/qa1931/_index.html
*/
Bluefruit.Advertising.restartOnDisconnect(true);
Bluefruit.Advertising.setInterval(32, 244); // in unit of 0.625 ms
Bluefruit.Advertising.setFastTimeout(30); // number of seconds in fast mode
Bluefruit.Advertising.start(0); // 0 = Don't stop advertising after n seconds
}
void connect_callback(uint16_t conn_handle)
{
// Get the reference to current connection
BLEConnection* connection = Bluefruit.Connection(conn_handle);
char central_name[32] = { 0 };
connection->getPeerName(central_name, sizeof(central_name));
Serial.print("Connected to ");
Serial.println(central_name);
Serial.println("Please select the 'Neopixels' tab, click 'Connect' and have fun");
}
void loop()
{
// Echo received data
if ( Bluefruit.connected() && bleuart.notifyEnabled() )
{
int command = bleuart.read();
switch (command) {
case 'V': { // Get Version
commandVersion();
break;
}
case 'S': { // Setup dimensions, components, stride...
commandSetup();
break;
}
case 'C': { // Clear with color
commandClearColor();
break;
}
case 'B': { // Set Brightness
commandSetBrightness();
break;
}
case 'P': { // Set Pixel
commandSetPixel();
break;
}
case 'I': { // Receive new image
commandImage();
break;
}
}
}
}
void swapBuffers()
{
uint8_t *base_addr = pixelBuffer;
int pixelIndex = 0;
for (int j = 0; j < height; j++)
{
for (int i = 0; i < width; i++) {
if (components == 3) {
neopixel.setPixelColor(pixelIndex, neopixel.Color(*base_addr, *(base_addr+1), *(base_addr+2)));
}
else {
neopixel.setPixelColor(pixelIndex, neopixel.Color(*base_addr, *(base_addr+1), *(base_addr+2), *(base_addr+3) ));
}
base_addr+=components;
pixelIndex++;
}
pixelIndex += stride - width; // Move pixelIndex to the next row (take into account the stride)
}
neopixel.show();
}
void commandVersion() {
Serial.println(F("Command: Version check"));
sendResponse(NEOPIXEL_VERSION_STRING);
}
void commandSetup() {
Serial.println(F("Command: Setup"));
width = bleuart.read();
height = bleuart.read();
stride = bleuart.read();
componentsValue = bleuart.read();
is400Hz = bleuart.read();
neoPixelType pixelType;
pixelType = componentsValue + (is400Hz ? NEO_KHZ400 : NEO_KHZ800);
components = (componentsValue == NEO_RGB || componentsValue == NEO_RBG || componentsValue == NEO_GRB || componentsValue == NEO_GBR || componentsValue == NEO_BRG || componentsValue == NEO_BGR) ? 3:4;
Serial.printf("\tsize: %dx%d\n", width, height);
Serial.printf("\tstride: %d\n", stride);
Serial.printf("\tpixelType %d\n", pixelType);
Serial.printf("\tcomponents: %d\n", components);
if (pixelBuffer != NULL) {
delete[] pixelBuffer;
}
uint32_t size = width*height;
pixelBuffer = new uint8_t[size*components];
neopixel.updateLength(size);
neopixel.updateType(pixelType);
neopixel.setPin(PIN);
// Done
sendResponse("OK");
}
void commandSetBrightness() {
Serial.println(F("Command: SetBrightness"));
// Read value
uint8_t brightness = bleuart.read();
// Set brightness
neopixel.setBrightness(brightness);
// Refresh pixels
swapBuffers();
// Done
sendResponse("OK");
}
void commandClearColor() {
Serial.println(F("Command: ClearColor"));
// Read color
uint8_t color[MAXCOMPONENTS];
for (int j = 0; j < components;) {
if (bleuart.available()) {
color[j] = bleuart.read();
j++;
}
}
// Set all leds to color
int size = width * height;
uint8_t *base_addr = pixelBuffer;
for (int i = 0; i < size; i++) {
for (int j = 0; j < components; j++) {
*base_addr = color[j];
base_addr++;
}
}
// Swap buffers
Serial.println(F("ClearColor completed"));
swapBuffers();
if (components == 3) {
Serial.printf("\tclear (%d, %d, %d)\n", color[0], color[1], color[2] );
}
else {
Serial.printf("\tclear (%d, %d, %d, %d)\n", color[0], color[1], color[2], color[3] );
}
// Done
sendResponse("OK");
}
void commandSetPixel() {
Serial.println(F("Command: SetPixel"));
// Read position
uint8_t x = bleuart.read();
uint8_t y = bleuart.read();
// Read colors
uint32_t pixelOffset = y*width+x;
uint32_t pixelDataOffset = pixelOffset*components;
uint8_t *base_addr = pixelBuffer+pixelDataOffset;
for (int j = 0; j < components;) {
if (bleuart.available()) {
*base_addr = bleuart.read();
base_addr++;
j++;
}
}
// Set colors
uint32_t neopixelIndex = y*stride+x;
uint8_t *pixelBufferPointer = pixelBuffer + pixelDataOffset;
uint32_t color;
if (components == 3) {
color = neopixel.Color( *pixelBufferPointer, *(pixelBufferPointer+1), *(pixelBufferPointer+2) );
Serial.printf("\tcolor (%d, %d, %d)\n",*pixelBufferPointer, *(pixelBufferPointer+1), *(pixelBufferPointer+2) );
}
else {
color = neopixel.Color( *pixelBufferPointer, *(pixelBufferPointer+1), *(pixelBufferPointer+2), *(pixelBufferPointer+3) );
Serial.printf("\tcolor (%d, %d, %d, %d)\n", *pixelBufferPointer, *(pixelBufferPointer+1), *(pixelBufferPointer+2), *(pixelBufferPointer+3) );
}
neopixel.setPixelColor(neopixelIndex, color);
neopixel.show();
// Done
sendResponse("OK");
}
void commandImage() {
Serial.printf("Command: Image %dx%d, %d, %d\n", width, height, components, stride);
// Receive new pixel buffer
int size = width * height;
uint8_t *base_addr = pixelBuffer;
for (int i = 0; i < size; i++) {
for (int j = 0; j < components;) {
if (bleuart.available()) {
*base_addr = bleuart.read();
base_addr++;
j++;
}
}
/*
if (components == 3) {
uint32_t index = i*components;
Serial.printf("\tp%d (%d, %d, %d)\n", i, pixelBuffer[index], pixelBuffer[index+1], pixelBuffer[index+2] );
}
*/
}
// Swap buffers
Serial.println(F("Image received"));
swapBuffers();
// Done
sendResponse("OK");
}
void sendResponse(char const *response) {
Serial.printf("Send Response: %s\n", response);
bleuart.write(response, strlen(response)*sizeof(char));
}
Hi there,
The only questions are ,Which Board Support Package are you using?
Did you load the Adafruit Bootloader?
You may want to stick to getting the LED over bLE example working. then get more creative after that.
A good way is to provide the compiler output snips, (first 5 lines) and the last 20 b4 it uplaods the sketch.
HTH
GL
PJ
Board: I want to use XIAO nRF52840 Sense
How to lead the adafruit bootloader?
Do you have any LED examples for this board? I got working code for XIAO mbed enabled nRF52840 Sense.
like this?
with this code…
/*
MIT License
THE SOFTWARE IS PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE AND NONINFRINGEMENT. IN NO EVENT SHALL THE AUTHORS OR COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE.
*/
/*
* Seeed XIAO BLE to control a WS2812B LED strip.
*/
#include <Adafruit_NeoPixel.h>
#define PIN D0
#define NUMPIXELS 12
#define DELAY 5 // 5ms between each hue change
uint16_t current_hue = 0; // in each loop call, the hue of the led strip color will be increased by 1
Adafruit_NeoPixel pixels(NUMPIXELS, PIN, NEO_GRB + NEO_KHZ800); // neo pixel object that is used to control the LED strip
void setup() {
pixels.begin();
}
void loop() {
current_hue = current_hue + 1; // In order to change the hue of the WS2812B LED strip, the hue i increased.
for (int i = 0; i < NUMPIXELS; ++i) { // iterate over all pixels
pixels.setPixelColor(i, pixels.ColorHSV(current_hue, 255, 255)); // set color of pixel
}
pixels.show();
delay(DELAY); // wait for 5ms
}
GL
PJ