Noob here, need help thinking out a new application/product

Hi all, I want make a logging pressure sensor. it would be for an automotive application to sense and log fuel pressure over a short period of time like 30secs. the sensor it self will screw in to a 1/8" NPT port, output a 0-5V signal dependent on pressure, 0 -15PSI. It would need to be able to record 10 times per second. it would store the readings on a usb key which would then be read on a laptop or similar device.

There is a follow on application, similar to this but reading 0-100 PSI for the same time period.

I might need to write up a little script that would dump the readings into a .XLS file or similar format. Even a CSV file would work.

I see there a new ADC board being advertised. Any bright ideas, suggestions, etc?