No sound when playing .wav in Python

Hi,

This is my first seeed project. I am using a ReSpeaker 2-Mics Pi HAT V1 on a Raspberry Pi 4

I recorded a wav file using ‘arecord’ , which I hear ok when I run : aplay -D “plughw:3,0” test.wav

But I am unable to hear the same wav file using python (see code below). The program pauses slightly which makes me think it is playing the file,. Do I need to increase the volume , or edit the asound.conf ?

I choose 3 for output_device_index to match aplay above
I installed GitHub - respeaker/seeed-voicecard: 2 Mic Hat, 4 Mic Array, 6-Mic Circular Array Kit, and 4-Mic Linear Array Kit for Raspberry Pi , and SPI is enabled .

I listed the /etc/asound.conf below.

Thanks, Peter

def play_wav(wavename):

file_path = r"/home/pi/test.wav"
print(f"Playing wav file  :  {file_path}")
wf = wave.open(str(file_path), 'rb')
p = pyaudio.PyAudio()
stream = p.open(format = p.get_format_from_width(wf.getsampwidth()),
                    channels = wf.getnchannels(),
                    rate = wf.getframerate(),
                    output = True,
                    output_device_index = 3)
            

# read data (based on the chunk size)
data = wf.readframes(chunk)
# play stream (looping from beginning of file to the end)
while data:
    # writing to the stream is what *actually* plays the sound.
    stream.write(data)
    data = wf.readframes(chunk)

# cleanup stuff.
stream.close()    
p.terminate()

=================================================================
here is the /etc/asound.conf

The IPC key of dmix or dsnoop plugin must be unique

If 555555 or 666666 is used by other processes, use another one

use samplerate to resample as speexdsp resample is bad

defaults.pcm.rate_converter “samplerate”

pcm.!default {
type asym
playback.pcm “playback”
capture.pcm “capture”
}

pcm.playback {
type plug
slave.pcm “dmixed”
}

pcm.capture {
type plug
slave.pcm “array”
}

pcm.dmixed {
type dmix
slave.pcm “hw:seeed2micvoicec”
ipc_key 555555
}

pcm.array {
type dsnoop
slave {
pcm “hw:seeed2micvoicec”
channels 2
}
ipc_key 666666
}

I fixed the bug.

aplay -l shows index =3 :
card 3: seeed2micvoicec [seeed-2mic-voicecard], device 0: bcm2835-i2s-wm8960-hifi
but python log shows index =1
Index 1: seeed-2mic-voicecard: bcm2835-i2s-wm8960-hifi wm8960-hifi-0 (plughw:3,0)
So I changed my python code to use “1” , and now it works.
Should we use aplay - is it broken?