No correct driver installation (Win 8.1, library 1.7.9)

Hello,
I received the Wio Terminal and the game was running correct when i switched it on.
Then i installed library 1.7.9 into Arduino IDE 1.8.12 but the device manager showed up Seed Wio Terminal without an USB Port (incorrect driver installation).
I read the thread: “Can’t Install the Device Driver” and had done all advices without success.
( Loading from: https://github.com/Seeed-Studio/Signed_USB_Serial_Driver and install it
in “user dir\AppData\Local\Arduino15\packages\hardware\samd\1.7.9\drivers\Signed_USB_Serial_Driver)
The Device Manager told me that it found the Wio Terminal driver but that the hash value in the catalog-file is missing. (In the folder are: seed_usb_serial.cat size:17.065 seed_usb_serial.inf size: 10.503)
When i enter the bootloader mode (sliding the power on switch 2 times) i can load the blink program in the arduino IDE to the Wio Terminal ( The tools - port window show up com port 11 in this case)
But i have to enter every time the Bootloader mode if i want to load a program into Wio Terminal.
The device manager show me that the driver is not installed correctly.

with kind regards
Erik

Hi @Erik01

You must download the driver from the release page here: https://github.com/Seeed-Studio/Signed_USB_Serial_Driver/releases/tag/1.0.2

Hello @ansonhe97

thank you very much, it is working fine now.

with kind regards
Erik