Hi all,
I’m working with NFC shield, but I must to change the antenna’s shape.
I would like to know the following antenna’s parameters:
L value at 13.56 MHz
Q @13.56 MHz
I saw that the antenna dimension is 28mm X 30.5mm.
I would like to know conductor parameters:
• Width of tracks in mm
• Spacing between turns in mm
• Thickness of the conductor in µm
Thank you
Manuel
salman
December 17, 2019, 4:31am
2
Hi,
Do you want to use an external antenna for NFC? if not can you please more specific?
salmanfarisvp post_id=56880 time=1576557085 user_id=28399:
Hi,
Do you want to use an external antenna for NFC? if not can you please more specific?
Yes, I do. I need to change antenna’s shape, so I would like to know some information about the initial Antenna.
Can you help me?
Thank you
Manuel
salman
December 18, 2019, 5:37am
4
Information about this antenna right?
Yes, right!
May you send me more informations?
Thanks
Manuel
salman
December 20, 2019, 10:48am
6
Hi,
Currently, the design files are not available, but I can provide you design guide for the exact NFC 13.56MHZ ANTENNA . Please let me know if it helps you.