New reTerminal, powers up with blank screen

Thanks for the reply. Yes, I am trying to use the seeed-python-reterminal library.

I was unfamiliar with evtest, but I installed it and this is the output:

No device specified, trying to scan all of /dev/input/event*
Available devices:
/dev/input/event0:	Riitek Micro Keyboard Mouse
/dev/input/event1:	Riitek Micro Keyboard
/dev/input/event2:	seeed-tp
/dev/input/event3:	Riitek Micro Keyboard Consumer Control
/dev/input/event4:	vc4
/dev/input/event5:	ST LIS3LV02DL Accelerometer
/dev/input/event6:	vc4
Select the device event number [0-6]:

I did not see the device to test, so I did not proceed.

I also ran i2cdetect -y 1. Here is the output of that:

     0  1  2  3  4  5  6  7  8  9  a  b  c  d  e  f
00:          -- -- -- -- -- -- -- -- -- -- -- -- -- 
10: -- -- -- -- -- -- -- -- -- UU -- -- -- -- -- -- 
20: -- -- -- -- -- -- -- -- -- UU -- -- -- -- -- -- 
30: -- -- -- -- -- -- -- -- 38 -- -- -- -- -- -- -- 
40: -- -- -- -- -- UU -- -- -- -- -- -- -- -- -- -- 
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 
70: -- -- -- -- -- -- -- --                         

Sorry, I have no idea what I’m looking at in those results! :slight_smile: