New Product Ideas: A "Pocket Computer" that can be developed at any time and place.

New Product Ideas:



A “Pocket Computer” that can be developed at any time and place.



Do you often have to use different computers because of office work, but because it is not the computer you are used to, it is not so easy to operate, and you need to repeatedly install some software and environment?

Are you new to programming, but because the installation of the environment is complicated and gave up?



If there is a product that solves your problem, which allows you to use your operating system no matter which computer you 're using, and has helped you install all the dependent development environment that you need.



Lets you just focus on the programming. Do you have any suggestions or predictions for this product? We will take your opinions and decide whether to produce!

Hi,

I have personal interested in the Pocket C.H.I.P. model, it can run full Linux, it comes with Wifi and Bluetooth which is very handy. another one is Pocketbeagle it will be very nice if it has a display and keyboard and network connection too.

It will in the form of a USB Drive instead of Single Board Computer such as Raspberry Pi. Does’t matter what computer you use, as long as you choose the USB drive as the boot option, you get to use your own Linux System

It will in the form of a USB Drive instead of Single Board Computer such as Raspberry Pi. Does’t matter what computer you use, as long as you choose the USB drive as the boot option, you get to use your own Linux System