I like the idea, especially the base plate I was asking for at Base plate to attach Grove devices. I hope this base plate is going to be available separately.
Now,
- Is the Arduino form-factor board the best option? It takes a lot of space.
- It is not clear if the Grove base shield is connected to the main Intel computer, to the Cortex-M0 MCU, or not connected at all.
- If the board is inside a re-computer case, is there enough space to connect the Grove plugs to the horizontal analog connectors?