Hi again,
I can’t set the speed link to the network at 1Gbs.
I checked in Windows - installed default in emmc - before to install linux.
Now I have linux - Debian 10.3.
Someone had this problems and now have a solution?
I checked with two routers:
Assus - RT-N66U C1
Huawei - HG8143A5
Look at screen shoot:
I think my problems is the UTP cable.
I have 3 UTP cable from routers (2m). Is not written anything on that but I think they are CAT-5.
I check with another cable what have connection at 1Gbs and my little board set the speed network at 1000Mbs.
So in conclusion is necessary to found a CAT-5e or better a CAT-6.
Thank you,