Hello,
I have the v1 Respeaker with 4-mic array. I need to figure out the specs for the mic (e.g., sensitivity and reference SPL). Does someone have the spec sheet with the exact part number used on the array, or does someone have the sensitivity/reference SPL data? I need to convert from dBV Output to db SPL Input.
Thanks!
Eric
Dear Customer
Please look at the link:<LINK_TEXT text="http://www.mouser.com/ds/2/218/SPU0414H … 28439.pdf
">http://www.mouser.com/ds/2/218/SPU0414HR5H-SB-28439.pdf
</LINK_TEXT>
Thanks!
seeed techsupport team 
jianghong
Hi,
can you please provide which MEMS microphones are in ReSpeaker 2 Mic Array HAT for Raspberry Pi?
Also, in which Respeaker are the best MEMS microphones? And which?
Br
Vedran