Need help with SD card available size

Need help with SD card available size

Hi there,



128G in theory , but we only test with 16G.


Thanks

best rgds
Bill

Hello,

I used a 32GB SD card and used Etcher to copy the Debian image but it only shows 4GB when running the image. How do I get it to see all 32GB?

Hi there,


I use the 8G card and then use the balenaEtcher burn the sd card. I use the df -h and can see the 8G space.


https://www.balena.io/etcher/

respeaker@v2:~$ df -h
Filesystem Size Used Avail Use% Mounted on
udev 426M 0 426M 0% /dev
tmpfs 99M 4.6M 94M 5% /run
/dev/mmcblk0p2 7.2G 2.9G 4.0G 42% /
tmpfs 493M 0 493M 0% /dev/shm
tmpfs 5.0M 4.0K 5.0M 1% /run/lock
tmpfs 493M 0 493M 0% /sys/fs/cgroup
tmpfs 99M 8.0K 99M 1% /run/user/1000
/dev/mmcblk0p1 100M 6.0K 100M 1% /media/respeaker/BOOT1

Thanks

best rgds
Bill

Hi Bill,

After I rebooted the respeaker it showed the correct SD card size when I
ran “df -h” So, it’s working fine now but required a reboot for some
reason.

Thanks for the quick response!
Regards,
Dean

Dean Weber
Mobile: 858-354-4466
LinkedIn: www.linkedin.com/in/deanweber

Hi Bill,

After I rebooted the respeaker it showed the correct SD card size when I
ran “df -h” So, it’s working fine now but required a reboot for some
reason.

Thanks for the quick response!
Regards,
Dean

Dean Weber
Mobile: 858-354-4466
LinkedIn: www.linkedin.com/in/deanweber