Multiple LiPo batteries on the LiPo Rider Pro?

When connected in parallell, the fuller battery will charge the emptier battery until a balance is reached. It’s important that before connecting them in parallell, they must have very similar voltage, otherwise a very large current will flow between them. Probably easiest to first charge all batteries full individually, then connect them in parallell. After that they’ll work as a single battery.