mtXControl - a Rainbowduino Editor By Tobi

Step H seems a bit ambiguous. Do I run the actual mtXcontrol program from linux command line? Or, am I supposed to load the mtXcontrol.pde sketch from the Processing IDE?

I’ve tried running the mtXcontrol.pde sketch from the Processing, but there’s errors because none of the classes are defined (eg. Matrix).
I’ve also tried running the mtXcontrol, but it doesn’t detect anything.

Also, when I upload the firmware, all LEDs go red. Should this be what happens?

My setup info:

  1. I’m on linux, using an arduino UNO and using a first generation rainbowduino.
  2. I’m using the 8X8 LED attatchment: GTM2088 ARGB-24 L12 LK 079