Hi there,
So I’m interested in this as well, Radar vs. IMU on a wearable by the patient. I doubt any firmware code can be changed AS I’m pretty sure it’s proprietary firmware. Let’s see what the Fellow Seeeder’s have to say…BUMP?
Hi!
I have purchased some MR60FDA2 modules too. I don’t think you can change that. Beside this, I am experiencing some issues with the module’s functionality. Specifically, the sensor outputs false positives (i.e., detects a fall) when a person is sitting on a chair at the edge of the fall detection area. Is anyone having a similar problem?
I’m trying to use this device in the bathroom of an asylum as a contribution to the safety of the elderly individuals, I wanna know how these variables (rect_XL , rect_XR, rect_ZF, rect_ZB) are set and how they interfire in the ps rocess.
Thee height is 2.3 m, sensitivity is 6 and threshold is 1.
The values get from the radar for the variables are all 0.3.
Best reggards,
Eduardo
So those are parameters for the BOX consider a detection ZONE if you will the object needs to pass through it or be in it AFAIK. Check the WIKI on the finer points and I pretty sure there is a thread on here about that.
if its on the ceiling be sure no LED or Light fixtures are near it.
You get it… lots of success has been reported but also with some angst to get it dialed in.
Hi Glasso, thanks for your help. I’ve already studied the content available in the Wiki. I tried to change these parameters using the GUI, but despite the instructions showing how to do that, it doesn’t work.
The current value is only 0.3 m, which is much too small for the detection area.
Ok, So I can say when I tested the Similar unit (mm/wave) , I had to do some strange connect at one Baud rate then Change it in the BLE trick/procedure for the App to work (the raw data is there), once I stumbled through it, You’ll see in the video posted, it worked well and was very accurate and repeatable.
There is also a Youtube video, with the setup and it’s working above a man in a chair He get’s up simulates the fall down and it’s detected as well as he is breathing kinda thing. It is an asian video not sure where but for a convention on medical devices.
More and more of these are coming out and so is the Science behind how they actually work, keep looking you’ll find it out. I’ll look and post back if I can find it too.
HTH
GL PJ
ps. the main take away was it had to be very sturdy mounted two or some inches below the ceiling (there’s a drawing in the wiki or datasheet for the sensor) and the detection box calibrated to be 2 inches off the floor with the far end of the measurement zone. if that makes sense.