Hello,
can someone help me to read the MR60FDA1 with an ESP8266 or ESP32. What pins should I use and do I need to do something in the code?
regards
Thomas_Dr
Hello,
can someone help me to read the MR60FDA1 with an ESP8266 or ESP32. What pins should I use and do I need to do something in the code?
regards
Thomas_Dr
ok, if I connect the sensor correctly, it works, with softserial.
regards
Thomas_Dr
You actually don’t need to use softserial for this, at least with an ESP32, you can just set it to Serial2 and either chose the pins or use pins 16/17 which are Serial 2 by default. Assuming you’re using the Seeed example code libraries with Arduino IDE. If you’re using the ESP with ESPHome, UART works the same as hardwareserial on Arduino… more or less.