Hi All,
With the Fall Detection Sensor - MR60FDA1, I tried the demo programs. Demo1 and Demo2 works. But Demo3 does not work. It does not show the effected data. I checked radar.sensor_report from radar.Fall_Detection() always being “0”. Is it caused by the recent update ?? please help
Yes, I tried to test it at a distance about 3m. But it only send out 0. According to the related document, it should send out other numbers, such as : #define NOFALL 0x08#define FALL 0x09#define NORESIDENT 0x10#define RESIDENCY 0x11
Also, when using the same sensor, just change the function to radar.HumanExis_Func(), the output values of radar.sensor_report are normal.
May I ask if you have stayed down during ‘Fall time’. The MR60FDA1 preset ‘Fall time’ is 30s, i.e. you need to stay in the fall state for 30s to trigger the fall data. If you get up within 30s, it will break the fall state, i.e. report 0.
Suggest you to check your own Fall time
![]()
you can also change your Fall time according to the following command.
![]()
You can change the fall sensitivity if the top 3m is mounted as previously described, and you still don’t have any fall data after falling and getting up again after ‘Fall time’
![]()
Where did you get these information from? It looks different than what I found in the seeed wiki for fall detection pro 60ghz. Link: https://files.seeedstudio.com/wiki/60GHzradar/60GHz_mmWave_Sensor_Fall_Detection_Module_Pro-Universal_Protocol.pdf
I’m dealing with the same issue actually, the function Fall_Detection don’t give me any response so I tried to send data to the radar, in the documentation I saw something like ‘switch fall monitoring function’.
When I do this, I’m not getting the expected response back:
The hex I’m sending is: {0x53, 0x59, 0x83, 0x00, 0x00, 0x01, 0x01, 0xD1, 0x54, 0x43}
Edit:
I do see below the page that the functionality with red fond and sky blue background are to be implemented. Any other suggestion why this code is not working, the serial monitor gives me zero output…
radar.Fall_Detection(); //Receive radar data and start processing
if(radar.sensor_report != 0x00){
switch(radar.sensor_report){
case NOFALL:
Serial.println("The sensor detects this movement is not a fall.");
Serial.println("----------------------------");
break;
case FALL:
Serial.println("The sensor detects a fall.");
Serial.println("----------------------------");
break;
case NORESIDENT:
Serial.println("The sensors did not detect anyone staying in place.");
Serial.println("----------------------------");
break;
case RESIDENCY:
Serial.println("The sensor detects someone staying in place.");
Serial.println("----------------------------");
break;
}
}