MR60BHA2 sleeping Monitor?

Hi,

i used MR60BHA1 for sleep monitoring, now i need a couple more sensors and wanted to upgrade to the mr60bha2, because of the nice size and formfactor and…well… it’s the new one

I read the getting started page and didn’t found any hint if this has sleep decoder too?

Is it capable to use the same funcs as the mr60bha1? and is it able to return point-cloud-data in [x,y] for imaging the data?

Greetings
Joe

Hi there, Joe…

Maybe Seeedineers :grin: can Comment but it looks to me that the LIB gives it away, in that “NO”, this one isn’t as full feature as the Older one. IMO it was more precise too. It does more sleep stuff according to the data sheet and some more Keywords in Library.

You could always UART them together and get the best of both and perhaps the benefits of the C6 too. :+1:

Let’s see if someone chimes in on it with this Bump. :crossed_fingers:
I also notice the PCB has more area for Radar signal.

HTH
GL :slight_smile: PJ :v:

I’m also interested in the MR60BHA2 for the same purpose. I’ve been testing it out but it seems like it loses the presense detection too frequently and so the breathing rate drops. Unless there’s something I can tweak with it, it appears to unreliable for me to use it as an alarm for low breathing rates.