Hi ,
I just got my MR24HPC1 mmWave kit , while trying to connect it to home assistant ,from the straight forward configuration that i get from using esp home , when i add configure it says :
That API line misses , but it got solve by using ImproBLE as the way to integrate it .
2.If i want to connect to my WiFi but via another ESP32 that works as Access Point and Client at the same way , so the topology is like this.
mmWave --------- ESP32 Client/AP ---------- ESP32 Client/AP ------------ WiFi Lan
will it still get detected by the Home Assistant , do I need any additional config ? since I dont think in this scenario the ImproBLE will get triggered since the device will be really far from my HomaAssistant server