stowp
1
Hi.
I have found the following library on internet:
on which pins should I connect sda, sda and int to connect a mpu9250 and bme280 to a stm32f103?
Tanks!
Marcelo.
Hi @stowp ,
It looks like the library can run on Arduino Pro Mini 3.3V 8MHz or Teensy 3.1.
I think we can use Arduino compatible board, but I haven’t checked yet.