Just recieved my mmWave Human Detection Sensor Kit and hooked it upto home assistant. I’m having an issue where Existence Energy and Motion Energy do not update. When the device boots I get an initial value and then it does not change. This results in the sensor detection presence but then not clearing.
Motion detection works, I can see it continually moving from motion to motionless etc but the Energy levels do not work.
I can get a new energy value from either power cycling or resetting via the switch in homeassistant.
Make sure that the version of ESP-IDF (Espressif IoT Development Framework) used in your ESPHome configuration is compatible with your ESP32-C3 board and the mmWave components.
How do you check this compatiblity?
I appear to have the same issue.
Presence information keeps returning ‘detected’ and ‘Existence Energy’ never changes. Also, when I change configuration settings these do not seem to do anything. On refresh of the page in Home Assistance, the values return to their default values.
‘Motion information’ keeps changing in the log between active and motionless every few seconds, although there is nobody in the room.
Hi there,
I’m no expert but do recall something about define’ing each Item function separately in the yamL
for ESp home to pick it up? ALso I would unplug it it for a solid ten minutes.(after)
and same with reading Leave it on for a few minutes before reading or sending any config.
HTH
GL PJ
I can confirm this issue. The body movement just stays at 1 and thus the presence state.
I have fiddled around with the device for days and also updated esphome to the latest version and used the same yaml that you referenced.
I am giving up on that kit and will buy a different sensor which is sad as I thought seeed studio is delivering quality.
I did the same. Went with the Aqara Presence Sensor FP2 MmWave and it works good enough. Not perfect (sometimes doesn’t detect me while in the room), but 95% correct.
Still have the Seeed one, and hoping to get it working also.
The Aqara is double the price, but at least it works.
If you have already confirmed the correct installation method, please ensure that the measurement environment is a single-person indoor space. Please check whether the Active reporting of presence information is constantly reporting the data below regardless of the presence of a person: Report: 0x53 0x59 0x80 0x01 0x00 0x01 0x01 sum 0x54 0x43
If it is, please try adjusting the sensitivity.
So the sensor works much better using one of the four presets and modifying the sensitivity. sensor is “sitting” on the thin side facing my daughter’s room, the idea is to keep lights on when she’s reading and not moving.
How should the sensor be orientated? sitting or large area facing the target?
My sensors still seem way too sensitive or they are broken. Even when laying straight down against the floor (which is pointed at the ground) I still get presence and motion detected. I have tried selecting the presets and adjusting sensitivity but it still doesnt work. I seriously regret my purchase and should have gotten the Aqara.
Hi there,
Sorry to hear your having issues , Do you have a picture you can post? Have you visually inspected them(not that you should be required to , but as a comment)
TY
GL PJ
Hi - has anyone solved this issue? It seems like a software issue in that the presence is just a flag that is toggles by the various sensor conditions. My device is stuck in “detected”. Have fiddled with sensitivity and thresholds with no success. I have followed installation instructions exactly. @Seeed_Seraphina any suggestions other than “read the documentation?”