Missing Drivers for Odyssey Blue (Not In Odyssey Library Driver Package)

The Odyssey Blue is missing several drivers listed below:

Not Available ACPI\INT3400\2&DABA3FF&1 The drivers for this device are not installed.
Not Available ACPI\INT3407\TPWR The drivers for this device are not installed.
PCI Data Acquisition and Signal Processing Controller PCI\VEN_8086&DEV_318C&SUBSYS_72708086&REV_03\3&11583659&0&01 The drivers for this device are not installed.

These are apparently not contained in the Windows 10 library driver package which I have downloaded from the “Getting Started” page link.

Can you please tell me where I can find these.

Many thanks

Solution is to install Intel Dynamic Platform and Thermal Framework from here
Direct link to driver