There is no one reason users migrate from Office 365 to Google Workspace. Various reasons can be possible for users to do this migration task. To migrate Office 365 to G Suite is an effortless way try Shoviv Microsoft 365 to Google Workspace Migration Tool. It doesn’t affect the folder hierarchy and meta properties of data. Moreover, users can create and run multiple jobs at a time without affecting the speed of the process. It also provides some advanced features such as a filter option, incremental facility, and many more.
For more understanding of its features, users can download and install its free demo version.
Read more - Microsoft 365 to Google Workspace Mailboxes Migration Software
This post was flagged by the community and is temporarily hidden.
If you are looking to migrate from Microsoft 365 to Google Workspace then you can use the native method. It is completely safe and you do not need to spend a single penny. All you need to have proper knowledge of the migration and you should be familiar with both platforms. It requires you to perform some steps manually. For reference, you can check out the below article. It will help you learn and perform the migration manually using native method.
If you want to switch your platform from Office 365 to Google Workspace account then you need a complete walkthrough. I have an amazing article that describes every single step to migrate Office 365 account to Google Workspace.
I totally recommend Gs Rochcopy360 to migrate from office to Google Workspace directly , it is easy and quick .